<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC812 can not work at 1.8V</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-can-not-work-at-1-8V/m-p/1670127#M53030</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Can you give us more information for example, how do you&amp;nbsp; know that the LPC812 does not work when the VDD is 2.6V?&lt;/P&gt;
&lt;P&gt;Pls use the LED blinky example in SDK and impress 2.6V to the VDD, does the LED still toggle?&lt;/P&gt;
&lt;P&gt;If the BOD is disabled, I do not think there is special configuration if you use low voltage VDD.&lt;/P&gt;
&lt;P&gt;In 2.6V, if you press Reset, can the board work?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Thu, 15 Jun 2023 09:15:12 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-06-15T09:15:12Z</dc:date>
    <item>
      <title>LPC812 can not work at 1.8V</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-can-not-work-at-1-8V/m-p/1670000#M53027</link>
      <description>&lt;P&gt;hello everyone,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;According to the user manual, lpc812 can work at 1.8v-3.6v, but the test results of my side will not work when th&lt;/SPAN&gt;&lt;SPAN&gt;e voltage is lower than 2.6v, and the BOD function is also disabled.&amp;nbsp;&lt;/SPAN&gt;Do I need any special Settings if I want to use 1.8v?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jun 2023 07:12:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-can-not-work-at-1-8V/m-p/1670000#M53027</guid>
      <dc:creator>wwz</dc:creator>
      <dc:date>2023-06-15T07:12:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 can not work at 1.8V</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-can-not-work-at-1-8V/m-p/1670127#M53030</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Can you give us more information for example, how do you&amp;nbsp; know that the LPC812 does not work when the VDD is 2.6V?&lt;/P&gt;
&lt;P&gt;Pls use the LED blinky example in SDK and impress 2.6V to the VDD, does the LED still toggle?&lt;/P&gt;
&lt;P&gt;If the BOD is disabled, I do not think there is special configuration if you use low voltage VDD.&lt;/P&gt;
&lt;P&gt;In 2.6V, if you press Reset, can the board work?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jun 2023 09:15:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-can-not-work-at-1-8V/m-p/1670127#M53030</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-06-15T09:15:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 can not work at 1.8V</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-can-not-work-at-1-8V/m-p/1670163#M53034</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the quick response, i have found the problem, it is caused by an external reset chip.but i have another quesiton: for the BOD reset level 0, LPC812 has no description of reset level 0 ,but LPC824 has the description of reset levle 0，Is it the same as LPC824?&lt;/P&gt;&lt;P&gt;thanks &amp;amp; best regards！&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jun 2023 09:46:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-can-not-work-at-1-8V/m-p/1670163#M53034</guid>
      <dc:creator>wwz</dc:creator>
      <dc:date>2023-06-15T09:46:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 can not work at 1.8V</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-can-not-work-at-1-8V/m-p/1670699#M53047</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that there is not reset level 0 for both LPC82x and LPC81x, there are Reset level 1,2,3, which corresponds to different Reset threshold voltage.&lt;/P&gt;
&lt;P&gt;For LPC81x:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1686881560166.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228020i9AB14B2F243A6927/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1686881560166.png" alt="xiangjun_rong_0-1686881560166.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The corresponding threshold voltage for LPC81x is defined in data sheet of LPC81x:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_1-1686881701544.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228021iBD2864ACC38ABD78/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_1-1686881701544.png" alt="xiangjun_rong_1-1686881701544.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 02:15:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-can-not-work-at-1-8V/m-p/1670699#M53047</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-06-16T02:15:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 can not work at 1.8V</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-can-not-work-at-1-8V/m-p/1670750#M53050</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;OK,&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 04:01:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-can-not-work-at-1-8V/m-p/1670750#M53050</guid>
      <dc:creator>wwz</dc:creator>
      <dc:date>2023-06-16T04:01:09Z</dc:date>
    </item>
  </channel>
</rss>