<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC2468 SDRAM change from Micron to ISSI problem.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468-SDRAM-change-from-Micron-to-ISSI-problem/m-p/1668430#M52986</link>
    <description>&lt;P&gt;We have a product that has been in series production since 2008-ish, using the &lt;STRONG&gt;LPC2468&lt;/STRONG&gt; together with a SDRAM Micron &lt;STRONG&gt;MT48LC4M32B2P-6A&lt;/STRONG&gt; without any problems.&lt;/P&gt;&lt;P&gt;Now, due to shortage of the Micron part, we have tried to use an ISSI part, &lt;STRONG&gt;IS42S32400F-6TLI&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;The problem is that we get, what appears to be, a random behaviour of the boards.&lt;BR /&gt;Sometimes they start just fine and sometimes they fail during boot.&lt;BR /&gt;The same board can start 20 times, and all of a sudden fail a few times.&lt;BR /&gt;If the board starts, it appears to be happy and continues to work well.&lt;BR /&gt;This is of course an urgent problem for us.&lt;BR /&gt;Some kind of timing issue I guess, but according to the datasheets we think it should work.&lt;BR /&gt;So far we have not been able to solve it.&lt;BR /&gt;Is there anyone out there that successfully uses this or similar combo of NXP-ISSI and can share their timing parameters?.&lt;/P&gt;&lt;P&gt;Kind regards&lt;BR /&gt;Hans&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jun 2023 13:08:24 GMT</pubDate>
    <dc:creator>HansHagglund</dc:creator>
    <dc:date>2023-06-13T13:08:24Z</dc:date>
    <item>
      <title>LPC2468 SDRAM change from Micron to ISSI problem.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468-SDRAM-change-from-Micron-to-ISSI-problem/m-p/1668430#M52986</link>
      <description>&lt;P&gt;We have a product that has been in series production since 2008-ish, using the &lt;STRONG&gt;LPC2468&lt;/STRONG&gt; together with a SDRAM Micron &lt;STRONG&gt;MT48LC4M32B2P-6A&lt;/STRONG&gt; without any problems.&lt;/P&gt;&lt;P&gt;Now, due to shortage of the Micron part, we have tried to use an ISSI part, &lt;STRONG&gt;IS42S32400F-6TLI&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;The problem is that we get, what appears to be, a random behaviour of the boards.&lt;BR /&gt;Sometimes they start just fine and sometimes they fail during boot.&lt;BR /&gt;The same board can start 20 times, and all of a sudden fail a few times.&lt;BR /&gt;If the board starts, it appears to be happy and continues to work well.&lt;BR /&gt;This is of course an urgent problem for us.&lt;BR /&gt;Some kind of timing issue I guess, but according to the datasheets we think it should work.&lt;BR /&gt;So far we have not been able to solve it.&lt;BR /&gt;Is there anyone out there that successfully uses this or similar combo of NXP-ISSI and can share their timing parameters?.&lt;/P&gt;&lt;P&gt;Kind regards&lt;BR /&gt;Hans&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 13:08:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468-SDRAM-change-from-Micron-to-ISSI-problem/m-p/1668430#M52986</guid>
      <dc:creator>HansHagglund</dc:creator>
      <dc:date>2023-06-13T13:08:24Z</dc:date>
    </item>
  </channel>
</rss>