<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC51U68 deep sleep SWD in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-deep-sleep-SWD/m-p/1668316#M52981</link>
    <description>&lt;P&gt;Hi, I'm using the LPC51U68 SDK version 2.9.0, and I tried the sample&amp;nbsp;lpcxpresso51u68_utick_wakeup.&lt;BR /&gt;After programming this sample, I'm not anymore able to connect the chip for reprogramming or mass erase (via MCUXpresso)&lt;BR /&gt;I'm using CMIS-DAP V2.263 on MCU-LINK debug probe&lt;BR /&gt;Why the SWD is not working? I searched on U68 documentation, but I have not found any info about.&lt;BR /&gt;This is very big issue, I need to have my application that at RESET/POWER ON enters in deep sleep, and awakes fron internal timer or external event (GPIO trigger), but in this case no further FW program/update is allowed!!&lt;BR /&gt;Could you help me? How to solve this trouble?&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jun 2023 10:18:05 GMT</pubDate>
    <dc:creator>abele_barbieri</dc:creator>
    <dc:date>2023-06-13T10:18:05Z</dc:date>
    <item>
      <title>LPC51U68 deep sleep SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-deep-sleep-SWD/m-p/1668316#M52981</link>
      <description>&lt;P&gt;Hi, I'm using the LPC51U68 SDK version 2.9.0, and I tried the sample&amp;nbsp;lpcxpresso51u68_utick_wakeup.&lt;BR /&gt;After programming this sample, I'm not anymore able to connect the chip for reprogramming or mass erase (via MCUXpresso)&lt;BR /&gt;I'm using CMIS-DAP V2.263 on MCU-LINK debug probe&lt;BR /&gt;Why the SWD is not working? I searched on U68 documentation, but I have not found any info about.&lt;BR /&gt;This is very big issue, I need to have my application that at RESET/POWER ON enters in deep sleep, and awakes fron internal timer or external event (GPIO trigger), but in this case no further FW program/update is allowed!!&lt;BR /&gt;Could you help me? How to solve this trouble?&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 10:18:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-deep-sleep-SWD/m-p/1668316#M52981</guid>
      <dc:creator>abele_barbieri</dc:creator>
      <dc:date>2023-06-13T10:18:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 deep sleep SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-deep-sleep-SWD/m-p/1668654#M52992</link>
      <description>&lt;P&gt;Hello, to recovery the board you need to put in ISP mode and erase&amp;nbsp; the flash.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 22:07:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-deep-sleep-SWD/m-p/1668654#M52992</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-06-13T22:07:12Z</dc:date>
    </item>
  </channel>
</rss>