<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Detect wakeup source after Deep Power-down in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Detect-wakeup-source-after-Deep-Power-down/m-p/1661557#M52820</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using Deep Sleep and Deep Power-down in our application. In both the wakeup can be triggered by RTC alarm and two GPIOs (Deep Sleep: PINT, Deep Power-down: dedicated wakeup pins).&lt;/P&gt;&lt;P&gt;I need to use Deep Power-down to minimize the power consumption for most of the time (Power-down is not an option since it drives all pins low). The problem is that I also need to know which wakeup source I can blame after the wakeup. In Deep Power-down a wakeup causes a chip reset which means I cannot use RTC general purpose registers to store the wakeup source data (I assume there's no time for using ISR before the reset occurs).&lt;/P&gt;&lt;P&gt;Is there any way I could see the wakeup source after waking up from Deep Power-down?&lt;/P&gt;&lt;P&gt;I'm using LPC55S28.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 01 Jun 2023 07:02:53 GMT</pubDate>
    <dc:creator>vanska</dc:creator>
    <dc:date>2023-06-01T07:02:53Z</dc:date>
    <item>
      <title>Detect wakeup source after Deep Power-down</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Detect-wakeup-source-after-Deep-Power-down/m-p/1661557#M52820</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using Deep Sleep and Deep Power-down in our application. In both the wakeup can be triggered by RTC alarm and two GPIOs (Deep Sleep: PINT, Deep Power-down: dedicated wakeup pins).&lt;/P&gt;&lt;P&gt;I need to use Deep Power-down to minimize the power consumption for most of the time (Power-down is not an option since it drives all pins low). The problem is that I also need to know which wakeup source I can blame after the wakeup. In Deep Power-down a wakeup causes a chip reset which means I cannot use RTC general purpose registers to store the wakeup source data (I assume there's no time for using ISR before the reset occurs).&lt;/P&gt;&lt;P&gt;Is there any way I could see the wakeup source after waking up from Deep Power-down?&lt;/P&gt;&lt;P&gt;I'm using LPC55S28.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 07:02:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Detect-wakeup-source-after-Deep-Power-down/m-p/1661557#M52820</guid>
      <dc:creator>vanska</dc:creator>
      <dc:date>2023-06-01T07:02:53Z</dc:date>
    </item>
    <item>
      <title>Re: Detect wakeup source after Deep Power-down</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Detect-wakeup-source-after-Deep-Power-down/m-p/1662343#M52838</link>
      <description>&lt;P&gt;Hi&amp;nbsp;vanska&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We can check general purpose always on domain data storage. I extract it from UM11126.If this doesn't help, please contact me again.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1685677592174.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/225988i0F71314E6495FA81/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1685677592174.png" alt="ZhangJennie_0-1685677592174.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;This is General purpose always on domain data storage.&lt;/P&gt;
&lt;P&gt;Remark: This register is managed and updated by the ROM boot and cannot be updated by any application.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 03:46:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Detect-wakeup-source-after-Deep-Power-down/m-p/1662343#M52838</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2023-06-02T03:46:55Z</dc:date>
    </item>
    <item>
      <title>Re: Detect wakeup source after Deep Power-down</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Detect-wakeup-source-after-Deep-Power-down/m-p/1668529#M52989</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/13026"&gt;@ZhangJennie&lt;/a&gt;!&lt;/P&gt;&lt;P&gt;I was already using AOREG1 storage for logging purposes but the problem was that it didn't provide information about which I/O caused the wakeup (indeed it shows if it was caused by the RTC alarm or some wakeup pin). But after taking another look at the user manual, I found the&amp;nbsp;WAKEIOCAUSE register which was the missing piece of the puzzle. Now it works perfectly!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="vanska_0-1686670536024.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227451i47574F0E1FBA1F46/image-size/medium?v=v2&amp;amp;px=400" role="button" title="vanska_0-1686670536024.png" alt="vanska_0-1686670536024.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 15:39:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Detect-wakeup-source-after-Deep-Power-down/m-p/1668529#M52989</guid>
      <dc:creator>vanska</dc:creator>
      <dc:date>2023-06-13T15:39:42Z</dc:date>
    </item>
  </channel>
</rss>