<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックWhen to use CMSIS peripheral driver?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/When-to-use-CMSIS-peripheral-driver/m-p/1659684#M52792</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Coming to plan my sw architecture and after going over the SDK examples I wonder&amp;nbsp;when should I use the standard&amp;nbsp;&lt;SPAN&gt;peripheral driver versus the CMSIS driver?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What's the considerations&amp;nbsp;when choosing between them?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Are they both updated?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Which of these two is more robust?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 30 May 2023 08:22:49 GMT</pubDate>
    <dc:creator>idof</dc:creator>
    <dc:date>2023-05-30T08:22:49Z</dc:date>
    <item>
      <title>When to use CMSIS peripheral driver?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/When-to-use-CMSIS-peripheral-driver/m-p/1659684#M52792</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Coming to plan my sw architecture and after going over the SDK examples I wonder&amp;nbsp;when should I use the standard&amp;nbsp;&lt;SPAN&gt;peripheral driver versus the CMSIS driver?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What's the considerations&amp;nbsp;when choosing between them?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Are they both updated?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Which of these two is more robust?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 30 May 2023 08:22:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/When-to-use-CMSIS-peripheral-driver/m-p/1659684#M52792</guid>
      <dc:creator>idof</dc:creator>
      <dc:date>2023-05-30T08:22:49Z</dc:date>
    </item>
    <item>
      <title>Re: When to use CMSIS peripheral driver?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/When-to-use-CMSIS-peripheral-driver/m-p/1660361#M52798</link>
      <description>&lt;P&gt;Hi&amp;nbsp;idof&amp;nbsp;&lt;/P&gt;
&lt;P&gt;CMSIS-Driver is ARM MDK Middleware.CMSIS-Driver is designed for multi semiconductor company products. NXP is one of the vendor&lt;BR /&gt;&lt;A href="https://www.keil.arm.com/devices" target="_blank"&gt;https://www.keil.arm.com/devices&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If user has requirement to port the code to other semiconductor device, using CMSIS driver would be easier.But please note, There are not many CMSIS demo released so far.&lt;BR /&gt;“ standard peripheral driver" are produced and mantained by NXP.&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 03:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/When-to-use-CMSIS-peripheral-driver/m-p/1660361#M52798</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2023-05-31T03:09:12Z</dc:date>
    </item>
  </channel>
</rss>