<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Maximum IO Voltage for LPC55S Family in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-IO-Voltage-for-LPC55S-Family/m-p/1659535#M52786</link>
    <description>&lt;P&gt;Hi&amp;nbsp;asarau&amp;nbsp;&lt;/P&gt;
&lt;P&gt;LPC55S6x can't operate at 1.8V with having 3.3V signal driven into the device. This will damage the device.&lt;BR /&gt;Table 11 is correct.&lt;BR /&gt;Table 24 defines the input voltage range but it must accord with Table 11 as well.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
    <pubDate>Tue, 30 May 2023 06:40:43 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2023-05-30T06:40:43Z</dc:date>
    <item>
      <title>Maximum IO Voltage for LPC55S Family</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-IO-Voltage-for-LPC55S-Family/m-p/1658585#M52756</link>
      <description>&lt;P&gt;I would like to operate the LPC55S6x series with a VCC of 1.8V and I am trying to figure out the maximum input voltage to the GPIO signals.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately the LPC55S6x datasheet provides two tables related to the maximum input voltage (VI) on IO pins programmed to provide a digital function, Table 11 and Table 24, that appear to conflict.&lt;/P&gt;&lt;P&gt;Table 24 indicates that the maximum input voltage for a device operating above 1.8V is 3.6V.&lt;/P&gt;&lt;P&gt;Table 11 indicates that the maximum input voltage for a device operating above 1.8V is VDD + 0.5V.&lt;/P&gt;&lt;P&gt;I believe that table 24 is correct, and a 3.3V signal may be driven into the LPC device when operating at 1.8V due to note 2 under table 11 that states: "Maximum/minimum voltage above the maximum operating voltage (see Table 24) ".&lt;/P&gt;&lt;P&gt;May the LPC55S6x operate at 1.8V while having a 3.3V signal driven into the device without damaging it?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 May 2023 19:17:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-IO-Voltage-for-LPC55S-Family/m-p/1658585#M52756</guid>
      <dc:creator>asarau</dc:creator>
      <dc:date>2023-05-26T19:17:55Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum IO Voltage for LPC55S Family</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-IO-Voltage-for-LPC55S-Family/m-p/1659535#M52786</link>
      <description>&lt;P&gt;Hi&amp;nbsp;asarau&amp;nbsp;&lt;/P&gt;
&lt;P&gt;LPC55S6x can't operate at 1.8V with having 3.3V signal driven into the device. This will damage the device.&lt;BR /&gt;Table 11 is correct.&lt;BR /&gt;Table 24 defines the input voltage range but it must accord with Table 11 as well.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Tue, 30 May 2023 06:40:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-IO-Voltage-for-LPC55S-Family/m-p/1659535#M52786</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2023-05-30T06:40:43Z</dc:date>
    </item>
  </channel>
</rss>