<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TDM Mode 0 Interfacing using Qualifier... in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/TDM-Mode-0-Interfacing-using-Qualifier/m-p/1657228#M52719</link>
    <description>&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;For example, the SGPIO Configuration intended were as follows in TX Mode 0:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - SGPIO8 - LRCLK&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - SGPIO9 - BCLK&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - SGPIO10 - DATAIN&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - SGPIO6 - DATAOUT&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lpestanas_0-1684983056706.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224771iB254AC7EA1D071D4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lpestanas_0-1684983056706.png" alt="lpestanas_0-1684983056706.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lpestanas_0-1684983056706.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If we were to use the qualifier enabled for LRCLK, are we able to frame the 32bit data without shifting by one bit? We would like to seek assistance on what would be the related registers to be initialized to achieve the syncing of LRCLK using the qualifier? And the clock source to be used is coming from PLL0Audio. We are not concerned about data justification (left/right). We just want a plain random binary data that will not shift by one bit.&lt;/P&gt;&lt;P&gt;Thanks and Good Day,&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;</description>
    <pubDate>Thu, 25 May 2023 03:09:14 GMT</pubDate>
    <dc:creator>lpestanas</dc:creator>
    <dc:date>2023-05-25T03:09:14Z</dc:date>
    <item>
      <title>TDM Mode 0 Interfacing using Qualifier...</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/TDM-Mode-0-Interfacing-using-Qualifier/m-p/1656069#M52681</link>
      <description>&lt;P&gt;Good Day,&lt;/P&gt;&lt;P&gt;We plan to implement a TDM Mode 0 between (2) LPC4300.&lt;/P&gt;&lt;P&gt;One will act as a Master and the other will act as a slave transmitting and receiving 32bit data.&lt;/P&gt;&lt;P&gt;We are facing an issue of missing out the bit 31 is always missed out upon the Falling edge of FSYNC pin. We are planning to use the qualifier to sync the 32bit-DATAIN and FSYNC. And&amp;nbsp;is it possible to have the FSYNC Data to trigger the qualifier on Rising Edge instead of Falling Edge?&lt;/P&gt;&lt;P&gt;Thanks and Good Day,&lt;/P&gt;&lt;P&gt;Leo Pestanas&lt;/P&gt;</description>
      <pubDate>Tue, 23 May 2023 23:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/TDM-Mode-0-Interfacing-using-Qualifier/m-p/1656069#M52681</guid>
      <dc:creator>lpestanas</dc:creator>
      <dc:date>2023-05-23T23:18:13Z</dc:date>
    </item>
    <item>
      <title>Re: TDM Mode 0 Interfacing using Qualifier...</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/TDM-Mode-0-Interfacing-using-Qualifier/m-p/1656213#M52686</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;In general, for I2S module, the DATAIN and FSYNC and SCK must be synchronized or from the same source, can you give more detailed information for the signal relationship among DATAIN and FSYNC and SCK signals&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 24 May 2023 03:47:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/TDM-Mode-0-Interfacing-using-Qualifier/m-p/1656213#M52686</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-05-24T03:47:57Z</dc:date>
    </item>
    <item>
      <title>Re: TDM Mode 0 Interfacing using Qualifier...</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/TDM-Mode-0-Interfacing-using-Qualifier/m-p/1657228#M52719</link>
      <description>&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;For example, the SGPIO Configuration intended were as follows in TX Mode 0:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - SGPIO8 - LRCLK&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - SGPIO9 - BCLK&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - SGPIO10 - DATAIN&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - SGPIO6 - DATAOUT&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lpestanas_0-1684983056706.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224771iB254AC7EA1D071D4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lpestanas_0-1684983056706.png" alt="lpestanas_0-1684983056706.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lpestanas_0-1684983056706.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If we were to use the qualifier enabled for LRCLK, are we able to frame the 32bit data without shifting by one bit? We would like to seek assistance on what would be the related registers to be initialized to achieve the syncing of LRCLK using the qualifier? And the clock source to be used is coming from PLL0Audio. We are not concerned about data justification (left/right). We just want a plain random binary data that will not shift by one bit.&lt;/P&gt;&lt;P&gt;Thanks and Good Day,&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;</description>
      <pubDate>Thu, 25 May 2023 03:09:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/TDM-Mode-0-Interfacing-using-Qualifier/m-p/1657228#M52719</guid>
      <dc:creator>lpestanas</dc:creator>
      <dc:date>2023-05-25T03:09:14Z</dc:date>
    </item>
    <item>
      <title>Re: TDM Mode 0 Interfacing using Qualifier...</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/TDM-Mode-0-Interfacing-using-Qualifier/m-p/1658299#M52749</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Regarding your question, I am not very clear.&lt;/P&gt;
&lt;P&gt;I suppose that you can get the SGPIO8 - LRCLK signal by shifting 4 words(32 bits each word), but only the MSB of first word is 1, all the other bits in 4 words are 0, is it okay?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 26 May 2023 09:39:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/TDM-Mode-0-Interfacing-using-Qualifier/m-p/1658299#M52749</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-05-26T09:39:59Z</dc:date>
    </item>
    <item>
      <title>Re: TDM Mode 0 Interfacing using Qualifier...</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/TDM-Mode-0-Interfacing-using-Qualifier/m-p/1660380#M52799</link>
      <description>&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;Yes, for example the channel data size is 32bits and start and end has an LRCLK Pulse invoked to mark the start and end of the transmission. For example, the data is 0010 0000 0000 0000 and to be transmitted. The receiving side sees 0001 0000 0000 0000 using Mode 0 TDM. What we are planning now is to make the LRCLK to be a GPIO instead of SGPIO to make the LRCLK more faster.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 03:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/TDM-Mode-0-Interfacing-using-Qualifier/m-p/1660380#M52799</guid>
      <dc:creator>lpestanas</dc:creator>
      <dc:date>2023-05-31T03:47:12Z</dc:date>
    </item>
  </channel>
</rss>