<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Deep sleep mode in LPC55S16</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Deep-sleep-mode-in-LPC55S16/m-p/1653614#M52583</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, you have to select or design the waking-up source, which can wake-up the LPC55S16 from deep-sleep mode.&lt;/P&gt;
&lt;P&gt;Pls refer to the section 14.4.5.3 Param2: wakeup_interrupts in UM11295.pdf&lt;/P&gt;
&lt;P&gt;For example, if you select the WAKEUP_GPIO_INT0_0, you have to design a hardware button on the PCB.&lt;/P&gt;
&lt;P&gt;If you select WAKEUP_CTIMER0, you do not require to do anything on the PCB.&lt;/P&gt;
&lt;P&gt;From software,the deep-sleep waking-up follows up the interrupt process, for example, you use WAKEUP_GPIO_INT0_0, you have to configure the PINT0&amp;nbsp; and select the pin, so that the pressing the pin can trigger an interrupt.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1684481123067.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/223931i888C9BE406735510/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1684481123067.png" alt="xiangjun_rong_0-1684481123067.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Pls refer to the an13166.pdf and corresponding firmware.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN13166.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN13166.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 19 May 2023 07:35:28 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-05-19T07:35:28Z</dc:date>
    <item>
      <title>Deep sleep mode in LPC55S16</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Deep-sleep-mode-in-LPC55S16/m-p/1653501#M52581</link>
      <description>&lt;P&gt;I need basic configuration to wake the controller from deep sleep mode on LPC 55S16. Any guidance?&lt;/P&gt;</description>
      <pubDate>Fri, 19 May 2023 04:12:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Deep-sleep-mode-in-LPC55S16/m-p/1653501#M52581</guid>
      <dc:creator>Balaji_KG</dc:creator>
      <dc:date>2023-05-19T04:12:53Z</dc:date>
    </item>
    <item>
      <title>Re: Deep sleep mode in LPC55S16</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Deep-sleep-mode-in-LPC55S16/m-p/1653614#M52583</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, you have to select or design the waking-up source, which can wake-up the LPC55S16 from deep-sleep mode.&lt;/P&gt;
&lt;P&gt;Pls refer to the section 14.4.5.3 Param2: wakeup_interrupts in UM11295.pdf&lt;/P&gt;
&lt;P&gt;For example, if you select the WAKEUP_GPIO_INT0_0, you have to design a hardware button on the PCB.&lt;/P&gt;
&lt;P&gt;If you select WAKEUP_CTIMER0, you do not require to do anything on the PCB.&lt;/P&gt;
&lt;P&gt;From software,the deep-sleep waking-up follows up the interrupt process, for example, you use WAKEUP_GPIO_INT0_0, you have to configure the PINT0&amp;nbsp; and select the pin, so that the pressing the pin can trigger an interrupt.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1684481123067.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/223931i888C9BE406735510/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1684481123067.png" alt="xiangjun_rong_0-1684481123067.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Pls refer to the an13166.pdf and corresponding firmware.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN13166.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN13166.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 May 2023 07:35:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Deep-sleep-mode-in-LPC55S16/m-p/1653614#M52583</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-05-19T07:35:28Z</dc:date>
    </item>
  </channel>
</rss>