<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: How to set LPC5516 CANFD sample point to more than 70% when baudrate more than 4M?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-set-LPC5516-CANFD-sample-point-to-more-than-70-when/m-p/1651978#M52561</link>
    <description>&lt;P&gt;&lt;EM&gt;&amp;gt; Regarding your question, the sampling point of CAN receiver is dependent on the the cable length, the signal quality...,&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And proper termination.&lt;BR /&gt;The higher the baudrate, the more critical it becomes.&lt;BR /&gt;The bandwidth requirements are at least an order of magnitude higher than the nominal baudrate.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 17 May 2023 10:23:21 GMT</pubDate>
    <dc:creator>frank_m</dc:creator>
    <dc:date>2023-05-17T10:23:21Z</dc:date>
    <item>
      <title>How to set LPC5516 CANFD sample point to more than 70% when baudrate more than 4M?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-set-LPC5516-CANFD-sample-point-to-more-than-70-when/m-p/1649757#M52488</link>
      <description>&lt;P&gt;When set sample point more than 70%, there will be a Protocol error in data phase and an error frame will be transmitted. No such problem when data baudrate less than 4M.Sample point less than 70% works well.&lt;/P&gt;&lt;P&gt;MCU: LPC5516&lt;/P&gt;&lt;P&gt;CANFD transmitter: TJA1042/3&lt;/P&gt;&lt;P&gt;CANFD module clock: 80MHz&lt;/P&gt;&lt;P&gt;Comm interface: Kvaser Hybrid&lt;/P&gt;&lt;P&gt;BTW: LPC54616 with same configuration works well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 14 May 2023 10:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-set-LPC5516-CANFD-sample-point-to-more-than-70-when/m-p/1649757#M52488</guid>
      <dc:creator>wangyanjun</dc:creator>
      <dc:date>2023-05-14T10:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: How to set LPC5516 CANFD sample point to more than 70% when baudrate more than 4M?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-set-LPC5516-CANFD-sample-point-to-more-than-70-when/m-p/1649858#M52495</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For your application, you set the CAN baud rate as 4M, I suppose that it is a bit high.&lt;/P&gt;
&lt;P&gt;For the CAN bit sampling point, it is complicated to select the sampling point,.&lt;/P&gt;
&lt;P&gt;I attach the an1798.pdf, hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 03:19:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-set-LPC5516-CANFD-sample-point-to-more-than-70-when/m-p/1649858#M52495</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-05-15T03:19:03Z</dc:date>
    </item>
    <item>
      <title>Re: How to set LPC5516 CANFD sample point to more than 70% when baudrate more than 4M?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-set-LPC5516-CANFD-sample-point-to-more-than-70-when/m-p/1649887#M52496</link>
      <description>&lt;P&gt;I use CAN FD, and data phase baudrate set to 4M, nominal baudrate set to 1M.&lt;/P&gt;&lt;P&gt;As SAE J2284-5, CAN FD baudrate can be set to 500K/5M.&lt;/P&gt;&lt;P&gt;In my application, when set to 500K/5M, sample point more than 75%, it can transmit and receive messages, but there are some error frames generated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to confirm:&lt;/P&gt;&lt;P&gt;Is the LPC5516 support sample point &amp;gt;= 75%?&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 03:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-set-LPC5516-CANFD-sample-point-to-more-than-70-when/m-p/1649887#M52496</guid>
      <dc:creator>wangyanjun</dc:creator>
      <dc:date>2023-05-15T03:58:40Z</dc:date>
    </item>
    <item>
      <title>Re: How to set LPC5516 CANFD sample point to more than 70% when baudrate more than 4M?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-set-LPC5516-CANFD-sample-point-to-more-than-70-when/m-p/1651621#M52547</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Regarding your question, the sampling point of CAN receiver is dependent on the the cable length, the signal quality..., I suppose it is okay to set the sampling point more than 75%.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 17 May 2023 02:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-set-LPC5516-CANFD-sample-point-to-more-than-70-when/m-p/1651621#M52547</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-05-17T02:27:09Z</dc:date>
    </item>
    <item>
      <title>Re: How to set LPC5516 CANFD sample point to more than 70% when baudrate more than 4M?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-set-LPC5516-CANFD-sample-point-to-more-than-70-when/m-p/1651978#M52561</link>
      <description>&lt;P&gt;&lt;EM&gt;&amp;gt; Regarding your question, the sampling point of CAN receiver is dependent on the the cable length, the signal quality...,&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And proper termination.&lt;BR /&gt;The higher the baudrate, the more critical it becomes.&lt;BR /&gt;The bandwidth requirements are at least an order of magnitude higher than the nominal baudrate.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 17 May 2023 10:23:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-set-LPC5516-CANFD-sample-point-to-more-than-70-when/m-p/1651978#M52561</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2023-05-17T10:23:21Z</dc:date>
    </item>
  </channel>
</rss>