<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flashing and Debugging without using LPC4322 on LPC55S69 using SWD in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-and-Debugging-without-using-LPC4322-on-LPC55S69-using/m-p/1644233#M52379</link>
    <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your immediate response. I am actually implementing the LPC4322 on the board to act as a debugger for LPC55s69.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I had a followup question:&lt;/P&gt;&lt;P&gt;Why is the LPC4322 operating at 2.5V on the EVK? It is capable of operating at the same voltage as LPC55S69 (3.3V).&lt;/P&gt;&lt;P&gt;Any particular reason or requirement to operate LPC4322 at 2.5v?&amp;nbsp;&lt;/P&gt;&lt;P&gt;TIA&lt;/P&gt;</description>
    <pubDate>Thu, 04 May 2023 04:11:42 GMT</pubDate>
    <dc:creator>SrinathVelavan</dc:creator>
    <dc:date>2023-05-04T04:11:42Z</dc:date>
    <item>
      <title>Flashing and Debugging without using LPC4322 on LPC55S69 using SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-and-Debugging-without-using-LPC4322-on-LPC55S69-using/m-p/1643417#M52364</link>
      <description>&lt;P&gt;I am developing a custom board design using LPC55S69 as host MCU. In the EVK, the flash programming and debugging is done using LPC4322 as the Link 2 probe with LPC55S69.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to do the flash programming and debugging without using the LPC4322?? Why is the LPC4322 operating at 2.5V on the EVK when it is capable of operating at 3.3V like the LPC55S69?&lt;/P&gt;&lt;P&gt;FYI, I am implementing only the Serial Wire Debug(SWD) interface [ Pins PIO0_11 and PIO0_12]. Is it possible to debug using only the SWD on the LPC55S69? Any information regarding this would be much helpful.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;TIA&lt;/P&gt;&lt;P&gt;#lpc55s69 #lpc4322&lt;/P&gt;</description>
      <pubDate>Wed, 03 May 2023 06:21:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-and-Debugging-without-using-LPC4322-on-LPC55S69-using/m-p/1643417#M52364</guid>
      <dc:creator>SrinathVelavan</dc:creator>
      <dc:date>2023-05-03T06:21:04Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing and Debugging without using LPC4322 on LPC55S69 using SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-and-Debugging-without-using-LPC4322-on-LPC55S69-using/m-p/1643835#M52377</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I review your information and I hope this information could help you.&lt;/P&gt;
&lt;P&gt;The proposes of the EVK are only for evaluation and get all in one, and you have a point you do not need to put the LPC43, and that is right, you do not need to add this debugger OB.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For your new custom board, you will need an external debugger but do not worry this&amp;nbsp;&lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcu-link-debug-probe:MCU-LINK" target="_blank"&gt;MCU Link JTAG/SWD Debug Probe | NXP Semiconductors&lt;/A&gt;&amp;nbsp;is the cheapest debugger from NXP, but there is another option depending on your requirement,&amp;nbsp;&lt;A href="https://www.nxp.com/products/power-management/motor-and-solenoid-drivers/powertrain-and-engine-control/universal-multilink-development-interface:UMultilink" target="_blank"&gt;Universal Multilink Development Interface | NXP Semiconductors&lt;/A&gt;, or J-link Segger all of this support SWD interface.&lt;/P&gt;
&lt;P&gt;Let me know if you have doubts.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 03 May 2023 18:48:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-and-Debugging-without-using-LPC4322-on-LPC55S69-using/m-p/1643835#M52377</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-05-03T18:48:38Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing and Debugging without using LPC4322 on LPC55S69 using SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-and-Debugging-without-using-LPC4322-on-LPC55S69-using/m-p/1644233#M52379</link>
      <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your immediate response. I am actually implementing the LPC4322 on the board to act as a debugger for LPC55s69.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I had a followup question:&lt;/P&gt;&lt;P&gt;Why is the LPC4322 operating at 2.5V on the EVK? It is capable of operating at the same voltage as LPC55S69 (3.3V).&lt;/P&gt;&lt;P&gt;Any particular reason or requirement to operate LPC4322 at 2.5v?&amp;nbsp;&lt;/P&gt;&lt;P&gt;TIA&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 04:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-and-Debugging-without-using-LPC4322-on-LPC55S69-using/m-p/1644233#M52379</guid>
      <dc:creator>SrinathVelavan</dc:creator>
      <dc:date>2023-05-04T04:11:42Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing and Debugging without using LPC4322 on LPC55S69 using SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-and-Debugging-without-using-LPC4322-on-LPC55S69-using/m-p/1645004#M52404</link>
      <description>&lt;P&gt;Hello, I reviewed the Datasheet of this LPC this chart is the voltage of use, I do not about the design of the PCB in specific voltage.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1683232523429.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/221845i5A741AA6FF8CAD83/image-size/large?v=v2&amp;amp;px=999" role="button" title="Pavel_Hernandez_0-1683232523429.png" alt="Pavel_Hernandez_0-1683232523429.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pavel_Hernandez_0-1683232523429.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I recommend review the chapter&amp;nbsp;10.2 Peripheral power consumption&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/data-sheet/LPC435X_3X_2X_1X.pdf" target="_blank"&gt;LPC435x/3x/2x/1x Product Data Sheet (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Let me know if you have more doubts.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 20:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-and-Debugging-without-using-LPC4322-on-LPC55S69-using/m-p/1645004#M52404</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-05-04T20:53:11Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing and Debugging without using LPC4322 on LPC55S69 using SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-and-Debugging-without-using-LPC4322-on-LPC55S69-using/m-p/1645195#M52413</link>
      <description>&lt;P&gt;Thanks for your help. I will look into the peripheral power consumption chapter in the datasheet.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 May 2023 03:42:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-and-Debugging-without-using-LPC4322-on-LPC55S69-using/m-p/1645195#M52413</guid>
      <dc:creator>SrinathVelavan</dc:creator>
      <dc:date>2023-05-05T03:42:25Z</dc:date>
    </item>
  </channel>
</rss>