<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックFail to connect LPC5534 via SWD</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Fail-to-connect-LPC5534-via-SWD/m-p/1640348#M52317</link>
    <description>&lt;P&gt;I cannot connect to LPC5534 after program it the first time.&lt;BR /&gt;&lt;BR /&gt;Using&lt;BR /&gt;J Link+ Debugger V9.3&lt;BR /&gt;MCUXpresso IDE v11.5.1 [Build 7266]&lt;BR /&gt;LPC5534&lt;/P&gt;&lt;P&gt;After the first programming I cannot connect to the controller via J-Flash, J-Flash Lite (both 7.62c) or Ozone Debugger 3.28e. The internal bootloader starts the application which is running and available via Modbus Poll.&lt;BR /&gt;By trying to download a new program in the µC there is a reset behavior, but the programming is not possible.&lt;/P&gt;</description>
    <pubDate>Wed, 26 Apr 2023 08:02:14 GMT</pubDate>
    <dc:creator>LEGR</dc:creator>
    <dc:date>2023-04-26T08:02:14Z</dc:date>
    <item>
      <title>Fail to connect LPC5534 via SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Fail-to-connect-LPC5534-via-SWD/m-p/1640348#M52317</link>
      <description>&lt;P&gt;I cannot connect to LPC5534 after program it the first time.&lt;BR /&gt;&lt;BR /&gt;Using&lt;BR /&gt;J Link+ Debugger V9.3&lt;BR /&gt;MCUXpresso IDE v11.5.1 [Build 7266]&lt;BR /&gt;LPC5534&lt;/P&gt;&lt;P&gt;After the first programming I cannot connect to the controller via J-Flash, J-Flash Lite (both 7.62c) or Ozone Debugger 3.28e. The internal bootloader starts the application which is running and available via Modbus Poll.&lt;BR /&gt;By trying to download a new program in the µC there is a reset behavior, but the programming is not possible.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Apr 2023 08:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Fail-to-connect-LPC5534-via-SWD/m-p/1640348#M52317</guid>
      <dc:creator>LEGR</dc:creator>
      <dc:date>2023-04-26T08:02:14Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to connect LPC5534 via SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Fail-to-connect-LPC5534-via-SWD/m-p/1641066#M52324</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216400"&gt;@LEGR&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;How about enter ISP mode, then erase full chip, connect again.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;About detail refer to:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Regaining-debug-access-to-target-MCU/m-p/473923" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Regaining-debug-access-to-target-MCU/m-p/473923&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Apr 2023 02:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Fail-to-connect-LPC5534-via-SWD/m-p/1641066#M52324</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-04-27T02:08:26Z</dc:date>
    </item>
  </channel>
</rss>