<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: After using MCU-Link installer rev 3.108, only one MCU-Link device is listed (VCOM Port) in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/After-using-MCU-Link-installer-rev-3-108-only-one-MCU-Link/m-p/1636961#M52263</link>
    <description>&lt;P&gt;The latest firmware changes from HID to WinUSB, see &lt;A href="https://community.nxp.com/t5/Blogs/MCU-Link-changes-to-use-WinUSB-for-MCUXpresso-IDE-11-7-and/ba-p/1583488/jump-to/first-unread-message" target="_blank"&gt;https://community.nxp.com/t5/Blogs/MCU-Link-changes-to-use-WinUSB-for-MCUXpresso-IDE-11-7-and/ba-p/1583488/jump-to/first-unread-message&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 20 Apr 2023 07:13:43 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2023-04-20T07:13:43Z</dc:date>
    <item>
      <title>After using MCU-Link installer rev 3.108, only one MCU-Link device is listed (VCOM Port)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/After-using-MCU-Link-installer-rev-3-108-only-one-MCU-Link/m-p/1636944#M52262</link>
      <description>&lt;P&gt;I updated firmware on my MCU-Link Probe and after following the steps on&amp;nbsp;&lt;A href="https://www.nxp.com/document/guide/getting-started-with-the-mcu-link:GS-MCU-LINK" target="_blank" rel="noopener"&gt;https://www.nxp.com/document/guide/getting-started-with-the-mcu-link:GS-MCU-LINK&lt;/A&gt;&amp;nbsp;I noticed that only the VCOM port device was listed, instead of the 3 devices indicated on the tutorial.&lt;/P&gt;&lt;P&gt;Last year, when I first purchased a few MCU Link probes I used the&amp;nbsp;MCU-Link installer rev 2.263 and with this version, the 3 devices were listed, namely, VCOM, and 2 HID devices. So then, I proceed to compare the "drivers" folder of each version and I noticed the revision 2.263 package has an extra driver, the HID driver. I copied this driver to the "drivers" folder of the rev 3.108 package and upgraded firmware again, updated the drivers from the windows device manager and still the 2 HID devices were not shown.&lt;/P&gt;&lt;P&gt;So my question is, is the firmware included in rev3.108 package missing something so that the 2 HID devices are also listed? Do we actually need all the 3 devices to be listed? If not, why and why it was included in rev 2.263 but not in rev3.108.&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 07:02:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/After-using-MCU-Link-installer-rev-3-108-only-one-MCU-Link/m-p/1636944#M52262</guid>
      <dc:creator>killerqueen</dc:creator>
      <dc:date>2023-04-20T07:02:43Z</dc:date>
    </item>
    <item>
      <title>Re: After using MCU-Link installer rev 3.108, only one MCU-Link device is listed (VCOM Port)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/After-using-MCU-Link-installer-rev-3-108-only-one-MCU-Link/m-p/1636961#M52263</link>
      <description>&lt;P&gt;The latest firmware changes from HID to WinUSB, see &lt;A href="https://community.nxp.com/t5/Blogs/MCU-Link-changes-to-use-WinUSB-for-MCUXpresso-IDE-11-7-and/ba-p/1583488/jump-to/first-unread-message" target="_blank"&gt;https://community.nxp.com/t5/Blogs/MCU-Link-changes-to-use-WinUSB-for-MCUXpresso-IDE-11-7-and/ba-p/1583488/jump-to/first-unread-message&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 07:13:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/After-using-MCU-Link-installer-rev-3-108-only-one-MCU-Link/m-p/1636961#M52263</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-04-20T07:13:43Z</dc:date>
    </item>
  </channel>
</rss>