<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックlpcxpresso824-max</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpcxpresso824-max/m-p/1633241#M52204</link>
    <description>&lt;P&gt;I got a&amp;nbsp;lpcxpresso824-max, version 2.&amp;nbsp; I note that it has a JP3 on it, and it seems that the documents on line do not include this.&amp;nbsp; At nxp.com, the schematics and docs are for version 1 and need to be updated.&lt;/P&gt;&lt;P&gt;On my Windows 11 machine, the board showed up only as a drive, USB MSC.&amp;nbsp; This was also true when I plugged it into my Linux machine.&lt;/P&gt;&lt;P&gt;There were no directions or firmware that I could find for the LPC11U35 on nxp.com, but I found instructions on os.mbed.com,&amp;nbsp;&lt;A href="https://os.mbed.com/platforms/LPCXpresso824-MAX/" target="_blank"&gt;https://os.mbed.com/platforms/LPCXpresso824-MAX/&lt;/A&gt;&amp;nbsp;and updated the firmware using a Windows10 machine at home.&amp;nbsp; The board now shows up as a drive and USB_CDC on my Linux machine and I was able to use the LPC11U35 to program and debug the board, but still does not appear on my Windows11 machine.&lt;/P&gt;&lt;P&gt;This is the output of lsusb -v from my Linux machine.&lt;/P&gt;&lt;P&gt;Bus 001 Device 015: ID 0d28:0204 NXP ARM mbed&lt;BR /&gt;Device Descriptor:&lt;BR /&gt;bLength 18&lt;BR /&gt;bDescriptorType 1&lt;BR /&gt;bcdUSB 1.10&lt;BR /&gt;bDeviceClass 2 Communications&lt;BR /&gt;bDeviceSubClass 0&lt;BR /&gt;bDeviceProtocol 0&lt;BR /&gt;bMaxPacketSize0 8&lt;BR /&gt;idVendor 0x0d28 NXP&lt;BR /&gt;idProduct 0x0204 ARM mbed&lt;BR /&gt;bcdDevice 1.00&lt;BR /&gt;iManufacturer 1 MBED&lt;BR /&gt;iProduct 2 MBED CMSIS-DAP&lt;BR /&gt;iSerial 3 0824022111466540EC98929C&lt;BR /&gt;bNumConfigurations 1&lt;BR /&gt;Configuration Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 2&lt;BR /&gt;wTotalLength 0x007a&lt;BR /&gt;bNumInterfaces 4&lt;BR /&gt;bConfigurationValue 1&lt;BR /&gt;iConfiguration 0&lt;BR /&gt;bmAttributes 0x80&lt;BR /&gt;(Bus Powered)&lt;BR /&gt;MaxPower 500mA&lt;BR /&gt;Interface Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 4&lt;BR /&gt;bInterfaceNumber 0&lt;BR /&gt;bAlternateSetting 0&lt;BR /&gt;bNumEndpoints 2&lt;BR /&gt;bInterfaceClass 8 Mass Storage&lt;BR /&gt;bInterfaceSubClass 6 SCSI&lt;BR /&gt;bInterfaceProtocol 80 Bulk-Only&lt;BR /&gt;iInterface 7 USB_MSC&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x82 EP 2 IN&lt;BR /&gt;bmAttributes 2&lt;BR /&gt;Transfer Type Bulk&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 0&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x02 EP 2 OUT&lt;BR /&gt;bmAttributes 2&lt;BR /&gt;Transfer Type Bulk&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 0&lt;BR /&gt;Interface Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 4&lt;BR /&gt;bInterfaceNumber 1&lt;BR /&gt;bAlternateSetting 0&lt;BR /&gt;bNumEndpoints 1&lt;BR /&gt;bInterfaceClass 2 Communications&lt;BR /&gt;bInterfaceSubClass 2 Abstract (modem)&lt;BR /&gt;bInterfaceProtocol 1 AT-commands (v.25ter)&lt;BR /&gt;iInterface 4 USB_CDC&lt;BR /&gt;CDC Header:&lt;BR /&gt;bcdCDC 1.10&lt;BR /&gt;CDC Call Management:&lt;BR /&gt;bmCapabilities 0x03&lt;BR /&gt;call management&lt;BR /&gt;use DataInterface&lt;BR /&gt;bDataInterface 2&lt;BR /&gt;CDC ACM:&lt;BR /&gt;bmCapabilities 0x06&lt;BR /&gt;sends break&lt;BR /&gt;line coding and serial state&lt;BR /&gt;CDC Union:&lt;BR /&gt;bMasterInterface 1&lt;BR /&gt;bSlaveInterface 2&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x83 EP 3 IN&lt;BR /&gt;bmAttributes 3&lt;BR /&gt;Transfer Type Interrupt&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0010 1x 16 bytes&lt;BR /&gt;bInterval 32&lt;BR /&gt;Interface Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 4&lt;BR /&gt;bInterfaceNumber 2&lt;BR /&gt;bAlternateSetting 0&lt;BR /&gt;bNumEndpoints 2&lt;BR /&gt;bInterfaceClass 10 CDC Data&lt;BR /&gt;bInterfaceSubClass 0&lt;BR /&gt;bInterfaceProtocol 0&lt;BR /&gt;iInterface 5 USB_CDC1&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x04 EP 4 OUT&lt;BR /&gt;bmAttributes 2&lt;BR /&gt;Transfer Type Bulk&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 0&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x84 EP 4 IN&lt;BR /&gt;bmAttributes 2&lt;BR /&gt;Transfer Type Bulk&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 0&lt;BR /&gt;Interface Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 4&lt;BR /&gt;bInterfaceNumber 3&lt;BR /&gt;bAlternateSetting 0&lt;BR /&gt;bNumEndpoints 2&lt;BR /&gt;bInterfaceClass 3 Human Interface Device&lt;BR /&gt;bInterfaceSubClass 0&lt;BR /&gt;bInterfaceProtocol 0&lt;BR /&gt;iInterface 6 MBED CMSIS-DAP&lt;BR /&gt;HID Device Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 33&lt;BR /&gt;bcdHID 1.00&lt;BR /&gt;bCountryCode 0 Not supported&lt;BR /&gt;bNumDescriptors 1&lt;BR /&gt;bDescriptorType 34 Report&lt;BR /&gt;wDescriptorLength 33&lt;BR /&gt;Report Descriptors:&lt;BR /&gt;** UNAVAILABLE **&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x81 EP 1 IN&lt;BR /&gt;bmAttributes 3&lt;BR /&gt;Transfer Type Interrupt&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 1&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x01 EP 1 OUT&lt;BR /&gt;bmAttributes 3&lt;BR /&gt;Transfer Type Interrupt&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 1&lt;BR /&gt;Device Status: 0x0000&lt;BR /&gt;(Bus Powered)&lt;/P&gt;</description>
    <pubDate>Thu, 13 Apr 2023 14:37:42 GMT</pubDate>
    <dc:creator>Daniel_Robinson</dc:creator>
    <dc:date>2023-04-13T14:37:42Z</dc:date>
    <item>
      <title>lpcxpresso824-max</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpcxpresso824-max/m-p/1633241#M52204</link>
      <description>&lt;P&gt;I got a&amp;nbsp;lpcxpresso824-max, version 2.&amp;nbsp; I note that it has a JP3 on it, and it seems that the documents on line do not include this.&amp;nbsp; At nxp.com, the schematics and docs are for version 1 and need to be updated.&lt;/P&gt;&lt;P&gt;On my Windows 11 machine, the board showed up only as a drive, USB MSC.&amp;nbsp; This was also true when I plugged it into my Linux machine.&lt;/P&gt;&lt;P&gt;There were no directions or firmware that I could find for the LPC11U35 on nxp.com, but I found instructions on os.mbed.com,&amp;nbsp;&lt;A href="https://os.mbed.com/platforms/LPCXpresso824-MAX/" target="_blank"&gt;https://os.mbed.com/platforms/LPCXpresso824-MAX/&lt;/A&gt;&amp;nbsp;and updated the firmware using a Windows10 machine at home.&amp;nbsp; The board now shows up as a drive and USB_CDC on my Linux machine and I was able to use the LPC11U35 to program and debug the board, but still does not appear on my Windows11 machine.&lt;/P&gt;&lt;P&gt;This is the output of lsusb -v from my Linux machine.&lt;/P&gt;&lt;P&gt;Bus 001 Device 015: ID 0d28:0204 NXP ARM mbed&lt;BR /&gt;Device Descriptor:&lt;BR /&gt;bLength 18&lt;BR /&gt;bDescriptorType 1&lt;BR /&gt;bcdUSB 1.10&lt;BR /&gt;bDeviceClass 2 Communications&lt;BR /&gt;bDeviceSubClass 0&lt;BR /&gt;bDeviceProtocol 0&lt;BR /&gt;bMaxPacketSize0 8&lt;BR /&gt;idVendor 0x0d28 NXP&lt;BR /&gt;idProduct 0x0204 ARM mbed&lt;BR /&gt;bcdDevice 1.00&lt;BR /&gt;iManufacturer 1 MBED&lt;BR /&gt;iProduct 2 MBED CMSIS-DAP&lt;BR /&gt;iSerial 3 0824022111466540EC98929C&lt;BR /&gt;bNumConfigurations 1&lt;BR /&gt;Configuration Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 2&lt;BR /&gt;wTotalLength 0x007a&lt;BR /&gt;bNumInterfaces 4&lt;BR /&gt;bConfigurationValue 1&lt;BR /&gt;iConfiguration 0&lt;BR /&gt;bmAttributes 0x80&lt;BR /&gt;(Bus Powered)&lt;BR /&gt;MaxPower 500mA&lt;BR /&gt;Interface Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 4&lt;BR /&gt;bInterfaceNumber 0&lt;BR /&gt;bAlternateSetting 0&lt;BR /&gt;bNumEndpoints 2&lt;BR /&gt;bInterfaceClass 8 Mass Storage&lt;BR /&gt;bInterfaceSubClass 6 SCSI&lt;BR /&gt;bInterfaceProtocol 80 Bulk-Only&lt;BR /&gt;iInterface 7 USB_MSC&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x82 EP 2 IN&lt;BR /&gt;bmAttributes 2&lt;BR /&gt;Transfer Type Bulk&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 0&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x02 EP 2 OUT&lt;BR /&gt;bmAttributes 2&lt;BR /&gt;Transfer Type Bulk&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 0&lt;BR /&gt;Interface Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 4&lt;BR /&gt;bInterfaceNumber 1&lt;BR /&gt;bAlternateSetting 0&lt;BR /&gt;bNumEndpoints 1&lt;BR /&gt;bInterfaceClass 2 Communications&lt;BR /&gt;bInterfaceSubClass 2 Abstract (modem)&lt;BR /&gt;bInterfaceProtocol 1 AT-commands (v.25ter)&lt;BR /&gt;iInterface 4 USB_CDC&lt;BR /&gt;CDC Header:&lt;BR /&gt;bcdCDC 1.10&lt;BR /&gt;CDC Call Management:&lt;BR /&gt;bmCapabilities 0x03&lt;BR /&gt;call management&lt;BR /&gt;use DataInterface&lt;BR /&gt;bDataInterface 2&lt;BR /&gt;CDC ACM:&lt;BR /&gt;bmCapabilities 0x06&lt;BR /&gt;sends break&lt;BR /&gt;line coding and serial state&lt;BR /&gt;CDC Union:&lt;BR /&gt;bMasterInterface 1&lt;BR /&gt;bSlaveInterface 2&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x83 EP 3 IN&lt;BR /&gt;bmAttributes 3&lt;BR /&gt;Transfer Type Interrupt&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0010 1x 16 bytes&lt;BR /&gt;bInterval 32&lt;BR /&gt;Interface Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 4&lt;BR /&gt;bInterfaceNumber 2&lt;BR /&gt;bAlternateSetting 0&lt;BR /&gt;bNumEndpoints 2&lt;BR /&gt;bInterfaceClass 10 CDC Data&lt;BR /&gt;bInterfaceSubClass 0&lt;BR /&gt;bInterfaceProtocol 0&lt;BR /&gt;iInterface 5 USB_CDC1&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x04 EP 4 OUT&lt;BR /&gt;bmAttributes 2&lt;BR /&gt;Transfer Type Bulk&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 0&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x84 EP 4 IN&lt;BR /&gt;bmAttributes 2&lt;BR /&gt;Transfer Type Bulk&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 0&lt;BR /&gt;Interface Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 4&lt;BR /&gt;bInterfaceNumber 3&lt;BR /&gt;bAlternateSetting 0&lt;BR /&gt;bNumEndpoints 2&lt;BR /&gt;bInterfaceClass 3 Human Interface Device&lt;BR /&gt;bInterfaceSubClass 0&lt;BR /&gt;bInterfaceProtocol 0&lt;BR /&gt;iInterface 6 MBED CMSIS-DAP&lt;BR /&gt;HID Device Descriptor:&lt;BR /&gt;bLength 9&lt;BR /&gt;bDescriptorType 33&lt;BR /&gt;bcdHID 1.00&lt;BR /&gt;bCountryCode 0 Not supported&lt;BR /&gt;bNumDescriptors 1&lt;BR /&gt;bDescriptorType 34 Report&lt;BR /&gt;wDescriptorLength 33&lt;BR /&gt;Report Descriptors:&lt;BR /&gt;** UNAVAILABLE **&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x81 EP 1 IN&lt;BR /&gt;bmAttributes 3&lt;BR /&gt;Transfer Type Interrupt&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 1&lt;BR /&gt;Endpoint Descriptor:&lt;BR /&gt;bLength 7&lt;BR /&gt;bDescriptorType 5&lt;BR /&gt;bEndpointAddress 0x01 EP 1 OUT&lt;BR /&gt;bmAttributes 3&lt;BR /&gt;Transfer Type Interrupt&lt;BR /&gt;Synch Type None&lt;BR /&gt;Usage Type Data&lt;BR /&gt;wMaxPacketSize 0x0040 1x 64 bytes&lt;BR /&gt;bInterval 1&lt;BR /&gt;Device Status: 0x0000&lt;BR /&gt;(Bus Powered)&lt;/P&gt;</description>
      <pubDate>Thu, 13 Apr 2023 14:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpcxpresso824-max/m-p/1633241#M52204</guid>
      <dc:creator>Daniel_Robinson</dc:creator>
      <dc:date>2023-04-13T14:37:42Z</dc:date>
    </item>
  </channel>
</rss>