<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 FLEXCOMM Pins of LPC55S69</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/FLEXCOMM-Pins-of-LPC55S69/m-p/1628103#M52109</link>
    <description>&lt;P&gt;I am working on creating a custom device with LPC55S69 as Host MCU. For a peripheral that is interfaced with LPC55S69 on SPI interface, I have used Flexcomm 1 (Pins 13 &amp;amp; 14) as MOSI &amp;amp; MISO respectively and Flexcomm 3 ( Pin 7) for SSEL. Can we use 2 different Flexcomm interfaces (1 &amp;amp; 3) for the same peripheral or should all pins be in the same Flexcomm interface??&amp;nbsp;&lt;/P&gt;&lt;P&gt;#lpc55s69&lt;/P&gt;</description>
    <pubDate>Wed, 05 Apr 2023 08:12:51 GMT</pubDate>
    <dc:creator>SrinathVelavan</dc:creator>
    <dc:date>2023-04-05T08:12:51Z</dc:date>
    <item>
      <title>FLEXCOMM Pins of LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/FLEXCOMM-Pins-of-LPC55S69/m-p/1628103#M52109</link>
      <description>&lt;P&gt;I am working on creating a custom device with LPC55S69 as Host MCU. For a peripheral that is interfaced with LPC55S69 on SPI interface, I have used Flexcomm 1 (Pins 13 &amp;amp; 14) as MOSI &amp;amp; MISO respectively and Flexcomm 3 ( Pin 7) for SSEL. Can we use 2 different Flexcomm interfaces (1 &amp;amp; 3) for the same peripheral or should all pins be in the same Flexcomm interface??&amp;nbsp;&lt;/P&gt;&lt;P&gt;#lpc55s69&lt;/P&gt;</description>
      <pubDate>Wed, 05 Apr 2023 08:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/FLEXCOMM-Pins-of-LPC55S69/m-p/1628103#M52109</guid>
      <dc:creator>SrinathVelavan</dc:creator>
      <dc:date>2023-04-05T08:12:51Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXCOMM Pins of LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/FLEXCOMM-Pins-of-LPC55S69/m-p/1630733#M52164</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;All SPI signals must routed to the same Flexcomm instance.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Mon, 10 Apr 2023 21:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/FLEXCOMM-Pins-of-LPC55S69/m-p/1630733#M52164</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-04-10T21:16:35Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXCOMM Pins of LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/FLEXCOMM-Pins-of-LPC55S69/m-p/1631827#M52184</link>
      <description>&lt;P&gt;Thank you for your clarification. Will make the necessary changes&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 06:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/FLEXCOMM-Pins-of-LPC55S69/m-p/1631827#M52184</guid>
      <dc:creator>SrinathVelavan</dc:creator>
      <dc:date>2023-04-12T06:26:48Z</dc:date>
    </item>
  </channel>
</rss>