<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC55S69 EVK Board - SPI Testing</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Board-SPI-Testing/m-p/1628042#M52106</link>
    <description>&lt;P&gt;I am trying to test out the SPI interface on the LPC55S69 EVK board. Tried the spi_polling_b2b_transfer_master code from the SDK and the Master Start was successfully obtained with loop-back mechanism.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now, am looking to get the same output without the help of loopback mechanism. Any help on this will be much appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, Is the LPC55S69 and LPC4322FET100E connected together on the EVK? If so, what is the use of the LPC4322 on the EVK board?&lt;/P&gt;&lt;P&gt;#spi #lpc55s69&lt;/P&gt;</description>
    <pubDate>Wed, 05 Apr 2023 05:17:30 GMT</pubDate>
    <dc:creator>SrinathVelavan</dc:creator>
    <dc:date>2023-04-05T05:17:30Z</dc:date>
    <item>
      <title>LPC55S69 EVK Board - SPI Testing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Board-SPI-Testing/m-p/1628042#M52106</link>
      <description>&lt;P&gt;I am trying to test out the SPI interface on the LPC55S69 EVK board. Tried the spi_polling_b2b_transfer_master code from the SDK and the Master Start was successfully obtained with loop-back mechanism.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now, am looking to get the same output without the help of loopback mechanism. Any help on this will be much appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, Is the LPC55S69 and LPC4322FET100E connected together on the EVK? If so, what is the use of the LPC4322 on the EVK board?&lt;/P&gt;&lt;P&gt;#spi #lpc55s69&lt;/P&gt;</description>
      <pubDate>Wed, 05 Apr 2023 05:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Board-SPI-Testing/m-p/1628042#M52106</guid>
      <dc:creator>SrinathVelavan</dc:creator>
      <dc:date>2023-04-05T05:17:30Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 EVK Board - SPI Testing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Board-SPI-Testing/m-p/1628112#M52110</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;EVK board equipted On-board (Link2) Debug probe, LPC4322 is the MCU for the debug probe. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;On board LPC4322 is neither SPI master nor slave.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;LPC55 SPI communication.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The spi_polling_board2board_master example shows how to use spi driver as master to do board to board transfer with polling.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;n this example, one spi instance as master and another spi instance on othereboard as slave. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In order to run this demo, two LPCXpresso55s69 boards are needed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Apr 2023 08:18:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Board-SPI-Testing/m-p/1628112#M52110</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2023-04-05T08:18:09Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 EVK Board - SPI Testing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Board-SPI-Testing/m-p/1628117#M52112</link>
      <description>Thank you very much for the clarification. I ll try the same with the 2 EVKs.</description>
      <pubDate>Wed, 05 Apr 2023 08:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Board-SPI-Testing/m-p/1628117#M52112</guid>
      <dc:creator>SrinathVelavan</dc:creator>
      <dc:date>2023-04-05T08:37:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 EVK Board - SPI Testing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Board-SPI-Testing/m-p/1628118#M52113</link>
      <description>&lt;P&gt;In the second board, How do I configure it to be the slave in the polling code example?&lt;/P&gt;</description>
      <pubDate>Wed, 05 Apr 2023 08:39:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Board-SPI-Testing/m-p/1628118#M52113</guid>
      <dc:creator>SrinathVelavan</dc:creator>
      <dc:date>2023-04-05T08:39:12Z</dc:date>
    </item>
  </channel>
</rss>