<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What's the difference between EHCI, KHCI and LPC IP3511 USB controller drivers? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-EHCI-KHCI-and-LPC-IP3511-USB/m-p/1627308#M52104</link>
    <description>&lt;P&gt;Using LPC552x MCU and trying to implement a custom HID device on USB1 port, but am not clear on the difference between the controller options. The SDK has several options&lt;BR /&gt;USB_DEVICE_CONFIG_KHCI&lt;BR /&gt;USB_DEVICE_CONFIG_EHCI&lt;BR /&gt;USB_DEVICE_CONFIG_LPCIP3511FS&lt;/P&gt;&lt;P&gt;USB_DEVICE_CONFIG_LPCIP3511HS&lt;/P&gt;&lt;P&gt;however most examples seem to use one of the IP3511 options.&lt;/P&gt;&lt;P&gt;What's the practical difference between EHCI, KHCI amd LPC IP3511 drivers? For LPC552x does it matter?&lt;/P&gt;</description>
    <pubDate>Tue, 04 Apr 2023 05:23:55 GMT</pubDate>
    <dc:creator>andrewjfox</dc:creator>
    <dc:date>2023-04-04T05:23:55Z</dc:date>
    <item>
      <title>What's the difference between EHCI, KHCI and LPC IP3511 USB controller drivers?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-EHCI-KHCI-and-LPC-IP3511-USB/m-p/1627308#M52104</link>
      <description>&lt;P&gt;Using LPC552x MCU and trying to implement a custom HID device on USB1 port, but am not clear on the difference between the controller options. The SDK has several options&lt;BR /&gt;USB_DEVICE_CONFIG_KHCI&lt;BR /&gt;USB_DEVICE_CONFIG_EHCI&lt;BR /&gt;USB_DEVICE_CONFIG_LPCIP3511FS&lt;/P&gt;&lt;P&gt;USB_DEVICE_CONFIG_LPCIP3511HS&lt;/P&gt;&lt;P&gt;however most examples seem to use one of the IP3511 options.&lt;/P&gt;&lt;P&gt;What's the practical difference between EHCI, KHCI amd LPC IP3511 drivers? For LPC552x does it matter?&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 05:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-EHCI-KHCI-and-LPC-IP3511-USB/m-p/1627308#M52104</guid>
      <dc:creator>andrewjfox</dc:creator>
      <dc:date>2023-04-04T05:23:55Z</dc:date>
    </item>
    <item>
      <title>Re: What's the difference between EHCI, KHCI and LPC IP3511 USB controller drivers?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-EHCI-KHCI-and-LPC-IP3511-USB/m-p/1629776#M52148</link>
      <description>&lt;P&gt;HI&amp;nbsp;andrewjfox&amp;nbsp;&lt;/P&gt;
&lt;P&gt;EHCI is Enhanced Host Controller Interfaceis which is not NXP IP. It is for usb 2.0 specification. You can google it for more information.&lt;BR /&gt;KHCI is Kinetis USB controller IP.&lt;BR /&gt;LPC IP3511 is LPC USB controller IP.&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Fri, 07 Apr 2023 13:04:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-EHCI-KHCI-and-LPC-IP3511-USB/m-p/1629776#M52148</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2023-04-07T13:04:26Z</dc:date>
    </item>
  </channel>
</rss>