<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックML state monitor</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ML-state-monitor/m-p/1624056#M52064</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;To categorize the multiple states of the fan(ON, OFF, CLOG, FRICTION), I am using Application Software Pack - ML-based System State Monitor on LPCXpresso55S69.&lt;/P&gt;&lt;P&gt;On the validation dataset, the prediction accuracy percentage for the confusion matrix for all states is greater than 95%. The model, however, is unable to distinguish between the ON and CLOG states with great clarity when tested on a real-time dataset. The outcome alternates between two states. I saw in the Jupyter notebook that the model was trained by only using Ax, Ay, and Az data. I modified the input dataset&amp;nbsp;in the Jupyter-notebook to add more data by integrating Bx, By, and Bz data and deployed the model on the MCUXpresso IDE to obtain more accurate results on swinging states. Real-time test results showed an even worse outcome. All four states are not recognized.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What changes should be made in the IDE's source code so that it correctly interacts with the new model and processes real-time data?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you so much!&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;#LPCXpresso55s69 #ml_state_monitor_cm33&amp;nbsp;@https://community.nxp.com/t5/eIQ-Machine-Learning-Software/Application-Software-Pack-ML-based-System-State-Monitor/ta-p/1413290&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 29 Mar 2023 09:05:25 GMT</pubDate>
    <dc:creator>khinhtethtetaung25</dc:creator>
    <dc:date>2023-03-29T09:05:25Z</dc:date>
    <item>
      <title>ML state monitor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ML-state-monitor/m-p/1624056#M52064</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;To categorize the multiple states of the fan(ON, OFF, CLOG, FRICTION), I am using Application Software Pack - ML-based System State Monitor on LPCXpresso55S69.&lt;/P&gt;&lt;P&gt;On the validation dataset, the prediction accuracy percentage for the confusion matrix for all states is greater than 95%. The model, however, is unable to distinguish between the ON and CLOG states with great clarity when tested on a real-time dataset. The outcome alternates between two states. I saw in the Jupyter notebook that the model was trained by only using Ax, Ay, and Az data. I modified the input dataset&amp;nbsp;in the Jupyter-notebook to add more data by integrating Bx, By, and Bz data and deployed the model on the MCUXpresso IDE to obtain more accurate results on swinging states. Real-time test results showed an even worse outcome. All four states are not recognized.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What changes should be made in the IDE's source code so that it correctly interacts with the new model and processes real-time data?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you so much!&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;#LPCXpresso55s69 #ml_state_monitor_cm33&amp;nbsp;@https://community.nxp.com/t5/eIQ-Machine-Learning-Software/Application-Software-Pack-ML-based-System-State-Monitor/ta-p/1413290&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Mar 2023 09:05:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ML-state-monitor/m-p/1624056#M52064</guid>
      <dc:creator>khinhtethtetaung25</dc:creator>
      <dc:date>2023-03-29T09:05:25Z</dc:date>
    </item>
    <item>
      <title>Re: ML state monitor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ML-state-monitor/m-p/1625934#M52084</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207871"&gt;@khinhtethtetaung25&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It seems the same issue with thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/ML-based-monitor/m-p/1622709" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/ML-based-monitor/m-p/1622709&lt;/A&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 31 Mar 2023 09:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ML-state-monitor/m-p/1625934#M52084</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-03-31T09:09:52Z</dc:date>
    </item>
  </channel>
</rss>