<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Tips for dual core performance on LPC55S69?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Tips-for-dual-core-performance-on-LPC55S69/m-p/1622087#M52027</link>
    <description>&lt;P&gt;I&amp;nbsp;&lt;EM&gt;thought&amp;nbsp;&lt;/EM&gt;I saw an app note on optimizing dual-core performance on the LPC55S6x family, but I can't find anything now.&lt;/P&gt;&lt;P&gt;Does such a resource exist? What I'm mostly looking for is information on memory contention. I see that both cores share the same flash memory interface. What kind of performance is achievable with both cores running from flash? Does the second core need to be running from RAM to be useful?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Sun, 26 Mar 2023 23:49:15 GMT</pubDate>
    <dc:creator>scottm</dc:creator>
    <dc:date>2023-03-26T23:49:15Z</dc:date>
    <item>
      <title>Tips for dual core performance on LPC55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Tips-for-dual-core-performance-on-LPC55S69/m-p/1622087#M52027</link>
      <description>&lt;P&gt;I&amp;nbsp;&lt;EM&gt;thought&amp;nbsp;&lt;/EM&gt;I saw an app note on optimizing dual-core performance on the LPC55S6x family, but I can't find anything now.&lt;/P&gt;&lt;P&gt;Does such a resource exist? What I'm mostly looking for is information on memory contention. I see that both cores share the same flash memory interface. What kind of performance is achievable with both cores running from flash? Does the second core need to be running from RAM to be useful?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Sun, 26 Mar 2023 23:49:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Tips-for-dual-core-performance-on-LPC55S69/m-p/1622087#M52027</guid>
      <dc:creator>scottm</dc:creator>
      <dc:date>2023-03-26T23:49:15Z</dc:date>
    </item>
    <item>
      <title>Re: Tips for dual core performance on LPC55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Tips-for-dual-core-performance-on-LPC55S69/m-p/1622408#M52040</link>
      <description>&lt;P&gt;Hi&amp;nbsp;scottm&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For LPC55 dual core communication, I suggest you referring "LPC55xx/LPC55Sxx Dual Core Communication"&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12335.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12335.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;and "LPC55xx/LPC55Sxx Dual-Core Debug in MCUXpresso"&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12358.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12358.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 08:31:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Tips-for-dual-core-performance-on-LPC55S69/m-p/1622408#M52040</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2023-03-27T08:31:45Z</dc:date>
    </item>
    <item>
      <title>Re: Tips for dual core performance on LPC55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Tips-for-dual-core-performance-on-LPC55S69/m-p/1629361#M52133</link>
      <description>&lt;P&gt;Hi Jun,&lt;/P&gt;&lt;P&gt;I've read those, and AN12335 does mention running code from an alternate RAM bank for best performance.&lt;/P&gt;&lt;P&gt;What I'm looking for is more information on how to structure things when it's not feasible to run the whole thing from RAM, and what kind of performance hit I can expect. I don't see anything at all in NXP's docs about running both cores from flash, but I'm sure I've seen information somewhere about using both cores with FreeRTOS and I don't&amp;nbsp;&lt;EM&gt;think&lt;/EM&gt; that involved completely separate copies of the RTOS.&lt;/P&gt;&lt;P&gt;This seems like a big topic that ought to have a lot of discussion&amp;nbsp;&lt;EM&gt;somewhere&lt;/EM&gt;. If it's not in NXP's documentation, is there ARM documentation I should be reading instead?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;</description>
      <pubDate>Thu, 06 Apr 2023 21:24:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Tips-for-dual-core-performance-on-LPC55S69/m-p/1629361#M52133</guid>
      <dc:creator>scottm</dc:creator>
      <dc:date>2023-04-06T21:24:35Z</dc:date>
    </item>
    <item>
      <title>Re: Tips for dual core performance on LPC55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Tips-for-dual-core-performance-on-LPC55S69/m-p/1629787#M52149</link>
      <description>&lt;P&gt;HI&amp;nbsp;scottm&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I don't think this is a NXP documentation.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Apr 2023 13:19:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Tips-for-dual-core-performance-on-LPC55S69/m-p/1629787#M52149</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2023-04-07T13:19:34Z</dc:date>
    </item>
  </channel>
</rss>