<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC845 default state of an output GPIO port in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-default-state-of-an-output-GPIO-port/m-p/1621879#M52021</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Indeed, in the documentation there is no mention of the default state of an output GPIO port, however, the state of a port's output bits can be read from its SET register. Please refer to the &lt;EM&gt;12.6.1 Reading pin state&lt;/EM&gt; section of the user manual for more detail.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
    <pubDate>Fri, 24 Mar 2023 19:49:55 GMT</pubDate>
    <dc:creator>_Leo_</dc:creator>
    <dc:date>2023-03-24T19:49:55Z</dc:date>
    <item>
      <title>LPC845 default state of an output GPIO port</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-default-state-of-an-output-GPIO-port/m-p/1621806#M52020</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I have tried to find the answer what the state of a standard GPIO is when it is changed to an output?&lt;BR /&gt;I can find in the datasheet that per default a GPIO is an inpout with a weak pull-up. But what is the output state when I change this in the DIR[0:1] register and before is set the output?&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Fri, 24 Mar 2023 15:47:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-default-state-of-an-output-GPIO-port/m-p/1621806#M52020</guid>
      <dc:creator>tyassin1</dc:creator>
      <dc:date>2023-03-24T15:47:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 default state of an output GPIO port</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-default-state-of-an-output-GPIO-port/m-p/1621879#M52021</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Indeed, in the documentation there is no mention of the default state of an output GPIO port, however, the state of a port's output bits can be read from its SET register. Please refer to the &lt;EM&gt;12.6.1 Reading pin state&lt;/EM&gt; section of the user manual for more detail.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Fri, 24 Mar 2023 19:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-default-state-of-an-output-GPIO-port/m-p/1621879#M52021</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-03-24T19:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 default state of an output GPIO port</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-default-state-of-an-output-GPIO-port/m-p/1621896#M52022</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Thank you for the answer.&lt;BR /&gt;&lt;BR /&gt;I was more interested in what state the output will be when it is changed from input to output. As I have some devices with enable pins, where they turn ON withan active high. So I guess I can fix this with a "stong" pull-down and then when the GPIO is changed to an output I would guess that the output is low. But to be sure and also because I cannot find it stated anywhere, I just ask this question in this forum.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Mar 2023 20:18:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-default-state-of-an-output-GPIO-port/m-p/1621896#M52022</guid>
      <dc:creator>tyassin1</dc:creator>
      <dc:date>2023-03-24T20:18:12Z</dc:date>
    </item>
  </channel>
</rss>