<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 lpc832 PWM on multiple pins simultaneously</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc832-PWM-on-multiple-pins-simultaneously/m-p/1611085#M51832</link>
    <description>&lt;P&gt;Hi, I'm working with an LPC832 by itself on a custom board - it's not an evaluation kit; SDK version 2.13.0 from 1/18/23 - and I can't get more than one PWM signal to work at a time. &amp;nbsp;The one pin that does work works fine and as expected, but the two other pins I want to run PWM on don't send a signal: I'm using an oscilloscope to watch for them on the output pins. &amp;nbsp;All three are configured the same way.&lt;/P&gt;&lt;P&gt;I see in the Pins page, Peripherals panel the following section - see image - and now I'm wondering if only one PWM signal is allowed at a time. &amp;nbsp;Is that what is meant by "routable to 16 pins, 1 signal" in the attached image? &amp;nbsp;If not, how do I get more than one PWM signal simultaneously?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Tue, 07 Mar 2023 18:11:35 GMT</pubDate>
    <dc:creator>aaronm</dc:creator>
    <dc:date>2023-03-07T18:11:35Z</dc:date>
    <item>
      <title>lpc832 PWM on multiple pins simultaneously</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc832-PWM-on-multiple-pins-simultaneously/m-p/1611085#M51832</link>
      <description>&lt;P&gt;Hi, I'm working with an LPC832 by itself on a custom board - it's not an evaluation kit; SDK version 2.13.0 from 1/18/23 - and I can't get more than one PWM signal to work at a time. &amp;nbsp;The one pin that does work works fine and as expected, but the two other pins I want to run PWM on don't send a signal: I'm using an oscilloscope to watch for them on the output pins. &amp;nbsp;All three are configured the same way.&lt;/P&gt;&lt;P&gt;I see in the Pins page, Peripherals panel the following section - see image - and now I'm wondering if only one PWM signal is allowed at a time. &amp;nbsp;Is that what is meant by "routable to 16 pins, 1 signal" in the attached image? &amp;nbsp;If not, how do I get more than one PWM signal simultaneously?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 18:11:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc832-PWM-on-multiple-pins-simultaneously/m-p/1611085#M51832</guid>
      <dc:creator>aaronm</dc:creator>
      <dc:date>2023-03-07T18:11:35Z</dc:date>
    </item>
    <item>
      <title>Re: lpc832 PWM on multiple pins simultaneously</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc832-PWM-on-multiple-pins-simultaneously/m-p/1611391#M51842</link>
      <description>&lt;P&gt;Never mind. &amp;nbsp;I figured it out: I had too many "states" defined - bottom of the SCT peripheral configuration page - and those conditions were never reached. &amp;nbsp;I removed states "1" and "2" and combined all PWM Signals in state 0. &amp;nbsp;It now works as expected. &amp;nbsp;I'll be the first to admit I'm just poking around, here, and don't really know what I'm doing. &amp;nbsp;But at least it's now working.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2023-03-08 at 1.28.49 AM.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/213655iC4425FA4DD41A93C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot 2023-03-08 at 1.28.49 AM.png" alt="Screenshot 2023-03-08 at 1.28.49 AM.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Wed, 08 Mar 2023 06:33:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc832-PWM-on-multiple-pins-simultaneously/m-p/1611391#M51842</guid>
      <dc:creator>aaronm</dc:creator>
      <dc:date>2023-03-08T06:33:36Z</dc:date>
    </item>
  </channel>
</rss>