<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC844 DAC?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC844-DAC/m-p/1608486#M51786</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Simple question. Does the LPC844 have a DAC?&lt;BR /&gt;The ordering information say it is only LPC845, but going through the datasheet or manual in the pin configuration, nothing is written about this. It seems that both have the feature.&lt;BR /&gt;&lt;BR /&gt;thank you.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 02 Mar 2023 16:07:25 GMT</pubDate>
    <dc:creator>tyassin1</dc:creator>
    <dc:date>2023-03-02T16:07:25Z</dc:date>
    <item>
      <title>LPC844 DAC?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC844-DAC/m-p/1608486#M51786</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Simple question. Does the LPC844 have a DAC?&lt;BR /&gt;The ordering information say it is only LPC845, but going through the datasheet or manual in the pin configuration, nothing is written about this. It seems that both have the feature.&lt;BR /&gt;&lt;BR /&gt;thank you.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Mar 2023 16:07:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC844-DAC/m-p/1608486#M51786</guid>
      <dc:creator>tyassin1</dc:creator>
      <dc:date>2023-03-02T16:07:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC844 DAC?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC844-DAC/m-p/1608811#M51789</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;You are right, as the following ordering inf in data sheet of LPC84x, only LPC845 has the DAC module, the LPC844 does not have the DAC module.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1677807936517.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/213073iBF1E94640E011E3C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1677807936517.png" alt="xiangjun_rong_0-1677807936517.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1677807936517.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 01:47:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC844-DAC/m-p/1608811#M51789</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-03-03T01:47:24Z</dc:date>
    </item>
  </channel>
</rss>