<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Serial Communications with MBED LPC1768 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Serial-Communications-with-MBED-LPC1768/m-p/1607070#M51756</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently using the MBED LPC1768 Microcontroller in a project where I wish to communicate with either MBED studio or a terminal emulator such as CoolTerm however, the device does not communicate at all. At first I though it maybe a programming issue so I tried the same code on a NUCLEO-L476RG and It worked perfectly, both within MBED Studio and in CoolTerm. The code its self quite simply prints "hello" using printf inside an infinite while loop.&lt;/P&gt;&lt;P&gt;Additionally, windows intermittently does not recognise the device however, it does still appear as a storage device and I am still able to run programs that do not utilise printf or make use of the serial libraries found in MBED OS.&lt;/P&gt;&lt;P&gt;I just wondered if there is a solution to this issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;firmware version: 141212&lt;/P&gt;&lt;P&gt;MBED OS: 6.16&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;many thanks,&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;</description>
    <pubDate>Tue, 28 Feb 2023 18:49:57 GMT</pubDate>
    <dc:creator>AndrewJKnowles</dc:creator>
    <dc:date>2023-02-28T18:49:57Z</dc:date>
    <item>
      <title>Serial Communications with MBED LPC1768</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Serial-Communications-with-MBED-LPC1768/m-p/1607070#M51756</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently using the MBED LPC1768 Microcontroller in a project where I wish to communicate with either MBED studio or a terminal emulator such as CoolTerm however, the device does not communicate at all. At first I though it maybe a programming issue so I tried the same code on a NUCLEO-L476RG and It worked perfectly, both within MBED Studio and in CoolTerm. The code its self quite simply prints "hello" using printf inside an infinite while loop.&lt;/P&gt;&lt;P&gt;Additionally, windows intermittently does not recognise the device however, it does still appear as a storage device and I am still able to run programs that do not utilise printf or make use of the serial libraries found in MBED OS.&lt;/P&gt;&lt;P&gt;I just wondered if there is a solution to this issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;firmware version: 141212&lt;/P&gt;&lt;P&gt;MBED OS: 6.16&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;many thanks,&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;</description>
      <pubDate>Tue, 28 Feb 2023 18:49:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Serial-Communications-with-MBED-LPC1768/m-p/1607070#M51756</guid>
      <dc:creator>AndrewJKnowles</dc:creator>
      <dc:date>2023-02-28T18:49:57Z</dc:date>
    </item>
    <item>
      <title>Re: Serial Communications with MBED LPC1768</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Serial-Communications-with-MBED-LPC1768/m-p/1608176#M51775</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213410"&gt;@AndrewJKnowles&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;About the MBED, recommend you ask help from MBED website:&amp;nbsp;&lt;A href="https://forums.mbed.com/categories" target="_blank"&gt;https://forums.mbed.com/categories&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;there are MBED experts know MBED issue well.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Mar 2023 07:22:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Serial-Communications-with-MBED-LPC1768/m-p/1608176#M51775</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-03-02T07:22:14Z</dc:date>
    </item>
  </channel>
</rss>