<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1768 + GPDMA + SSP + Burst size + memory boundary/alignment</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-GPDMA-SSP-Burst-size-memory-boundary-alignment/m-p/522530#M5166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by solsal on Thu Aug 23 16:18:14 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC1768 + GPDMA + SSP + Burst size + memory boundary&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;please refer to UM10360 page:611&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;my question is around these items:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC1768 + GPDMA + Burst size + memory boundary/alignment&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;.................................................. .................................................. ...................&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;31.6.4 Address generation&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Address generation can be either incrementing or non-incrementing (address wrapping is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;not supported).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Some devices, especially memories, disallow burst accesses across certain address&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;boundaries. The DMA controller assumes that this is the case with any source or&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;destination area, which is configured for incrementing addressing. This boundary is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;assumed to be aligned with the specified burst size. For example, if the channel is set for&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;16-transfer burst to a 32-bit wide device then the boundary is 64-bytes aligned (that is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;address bits [5:0] equal 0). If a DMA burst is to cross one of these boundaries, then,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;instead of a burst, that transfer is split into separate AHB transactions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;31.6.4.1 Word-aligned transfers across a boundary&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The channel is configured for 16-transfer bursts, each transfer 32-bits wide, to a&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;destination for which address incrementing is enabled. The start address for the current&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;burst is 0x0C000024, the next boundary (calculated from the burst size and transfer&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;width) is 0x0C000040.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The transfer will be split into two AHB transactions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;• a 7-transfer burst starting at address 0x0C000024&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;• a 9-transfer burst starting at address 0x0C000040.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;================================================== ====&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. what do those paragraphs mean?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Q: How should this operation be done?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to send an array of 1024 bytes to SSP0( spi ) and receive 1024 bytes from it to another array of 1024 bytes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(send and receive are Simultaneous : this is a full duplex operation then which of M2P/P2M/M2M ???)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;( this is repeatedly done every 100ms )&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"SSP0(SPI) hardware is connected to another 8bit_uC_SPI"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;by using SSP0+GPDMA+BURST+ "two 1024 bytes array in sram"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;what is the exact solution for this question?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;( I studied the USER MANUAL UM10360 but it is not clear enough and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I didn't find clean information around this )&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;================================================== ====&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have already done this operation on ( AT91SAM7X256(master) + atmega32(slave) ) on keil(arm) + codevision(AVR)....&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;now I want to do this by ( LPC1768(master) + atmega32(slave) ) , but this&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;GPDMA+BURST+memory alignment .... is confusing thing.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;the slave device is working properly on previous design and I need to run Master(lpc1768) properly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;================================================== ====&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;please share your knowledge ,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/www.nxp.com/documents/user_manual/UM10360.pdf" target="test_blank"&gt;www.nxp.com/documents/user_manual/UM10360.pdf&lt;/A&gt; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:55:36 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:55:36Z</dc:date>
    <item>
      <title>LPC1768 + GPDMA + SSP + Burst size + memory boundary/alignment</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-GPDMA-SSP-Burst-size-memory-boundary-alignment/m-p/522530#M5166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by solsal on Thu Aug 23 16:18:14 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC1768 + GPDMA + SSP + Burst size + memory boundary&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;please refer to UM10360 page:611&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;my question is around these items:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC1768 + GPDMA + Burst size + memory boundary/alignment&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;.................................................. .................................................. ...................&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;31.6.4 Address generation&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Address generation can be either incrementing or non-incrementing (address wrapping is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;not supported).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Some devices, especially memories, disallow burst accesses across certain address&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;boundaries. The DMA controller assumes that this is the case with any source or&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;destination area, which is configured for incrementing addressing. This boundary is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;assumed to be aligned with the specified burst size. For example, if the channel is set for&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;16-transfer burst to a 32-bit wide device then the boundary is 64-bytes aligned (that is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;address bits [5:0] equal 0). If a DMA burst is to cross one of these boundaries, then,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;instead of a burst, that transfer is split into separate AHB transactions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;31.6.4.1 Word-aligned transfers across a boundary&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The channel is configured for 16-transfer bursts, each transfer 32-bits wide, to a&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;destination for which address incrementing is enabled. The start address for the current&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;burst is 0x0C000024, the next boundary (calculated from the burst size and transfer&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;width) is 0x0C000040.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The transfer will be split into two AHB transactions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;• a 7-transfer burst starting at address 0x0C000024&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;• a 9-transfer burst starting at address 0x0C000040.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;================================================== ====&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. what do those paragraphs mean?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Q: How should this operation be done?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to send an array of 1024 bytes to SSP0( spi ) and receive 1024 bytes from it to another array of 1024 bytes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(send and receive are Simultaneous : this is a full duplex operation then which of M2P/P2M/M2M ???)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;( this is repeatedly done every 100ms )&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"SSP0(SPI) hardware is connected to another 8bit_uC_SPI"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;by using SSP0+GPDMA+BURST+ "two 1024 bytes array in sram"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;what is the exact solution for this question?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;( I studied the USER MANUAL UM10360 but it is not clear enough and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I didn't find clean information around this )&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;================================================== ====&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have already done this operation on ( AT91SAM7X256(master) + atmega32(slave) ) on keil(arm) + codevision(AVR)....&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;now I want to do this by ( LPC1768(master) + atmega32(slave) ) , but this&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;GPDMA+BURST+memory alignment .... is confusing thing.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;the slave device is working properly on previous design and I need to run Master(lpc1768) properly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;================================================== ====&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;please share your knowledge ,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/www.nxp.com/documents/user_manual/UM10360.pdf" target="test_blank"&gt;www.nxp.com/documents/user_manual/UM10360.pdf&lt;/A&gt; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-GPDMA-SSP-Burst-size-memory-boundary-alignment/m-p/522530#M5166</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 + GPDMA + SSP + Burst size + memory boundary/alignment</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-GPDMA-SSP-Burst-size-memory-boundary-alignment/m-p/522531#M5167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by solsal on Fri Aug 24 02:12:56 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;reading the examples of code_bundle_lpc1768 available at nxp.com&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SSP examples ( for keil )&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;sspdma.uvproj&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;=================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;uint32_t DMAChannel_Init( uint32_t ChannelNum, uint32_t DMAMode )&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; if ( ChannelNum == 0 )&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SSP0DMADone = 0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPDMA-&amp;gt;IntTCClear = 0x01&amp;lt;&amp;lt;0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPDMA-&amp;gt;IntErrClr = 0x01&amp;lt;&amp;lt;0;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if ( DMAMode == M2P )&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; /* Ch0 set for M2P transfer from mempry to peripheral. */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH0-&amp;gt;CSrcAddr = SSP0_DMA_TX_SRC;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH0-&amp;gt;CDestAddr = SSP0_DMA_TX_DST;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; /* The burst size is set to 1, source and dest transfer width is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; 32 bits(word), Terminal Count Int enable */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH0-&amp;gt;CControl = (SSP_DMA_SIZE &amp;amp; 0x0FFF)|(0x00 &amp;lt;&amp;lt; 12) &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;|(0x00 &amp;lt;&amp;lt; 15)|(0x00 &amp;lt;&amp;lt; 18)|(0x00 &amp;lt;&amp;lt; 21)|(1 &amp;lt;&amp;lt; 26)|0x80000000;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;else if ( DMAMode == P2M )&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; /* Ch0 set for P2M transfer from peripheral to memory. */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH0-&amp;gt;CSrcAddr = SSP0_DMA_RX_SRC;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH0-&amp;gt;CDestAddr = SSP0_DMA_RX_DST;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; /* The burst size is set to 1. Terminal Count Int enable. */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH0-&amp;gt;CControl = (SSP_DMA_SIZE &amp;amp; 0x0FFF)|(0x00 &amp;lt;&amp;lt; 12) &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;|(0x00 &amp;lt;&amp;lt; 15)|(0x00 &amp;lt;&amp;lt; 18)|(0x00 &amp;lt;&amp;lt; 21)|(1 &amp;lt;&amp;lt; 27)|0x80000000;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;else&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; return ( FALSE );&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; }&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; else if ( ChannelNum == 1 )&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SSP1DMADone = 0;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPDMA-&amp;gt;IntTCClear = 0x01&amp;lt;&amp;lt;1;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPDMA-&amp;gt;IntErrClr = 0x01&amp;lt;&amp;lt;1;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if ( DMAMode == M2P )&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; /* Ch1 set for M2P transfer from mempry to peripheral. */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH1-&amp;gt;CSrcAddr = SSP1_DMA_TX_SRC;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH1-&amp;gt;CDestAddr = SSP1_DMA_TX_DST;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; /* The burst size is set to 1. Terminal Count Int enable. */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH1-&amp;gt;CControl = (SSP_DMA_SIZE &amp;amp; 0x0FFF)|(0x00 &amp;lt;&amp;lt; 12) &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;|(0x00 &amp;lt;&amp;lt; 15)|(0x00 &amp;lt;&amp;lt; 18)|(0x00 &amp;lt;&amp;lt; 21)|(1 &amp;lt;&amp;lt; 26)|0x80000000;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;else if ( DMAMode == P2M )&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; /* Ch1 set for P2M transfer from peripheral to memory. */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH1-&amp;gt;CSrcAddr = SSP1_DMA_RX_SRC;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH1-&amp;gt;CDestAddr = SSP1_DMA_RX_DST;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; /* The burst size is set to 1. Terminal Count Int enable. */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; LPC_GPDMACH1-&amp;gt;CControl = (SSP_DMA_SIZE &amp;amp; 0x0FFF)|(0x00 &amp;lt;&amp;lt; 12) &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;|(0x00 &amp;lt;&amp;lt; 15)|(0x00 &amp;lt;&amp;lt; 18)|(0x00 &amp;lt;&amp;lt; 21)|(1 &amp;lt;&amp;lt; 27)|0x80000000;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;else&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; return ( FALSE );&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; }&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; else&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;return ( FALSE );&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; }&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; return( TRUE );&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;///////////////////////////////////////////////////////////////////////////////&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;you see !&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC1768 is capable for only half duplex transfer for SSP/SPI&amp;nbsp; by GPDMA !&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;only one mode&amp;nbsp; (P2M&amp;nbsp; for receive data from SPI(MISO) to memory) or (M2P&amp;nbsp; for sending data from memory to SPI (MOSI) ) !&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;isn't it confusing ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SPI is a full duplex peripheral.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;and it should be considered in GPDMA&amp;nbsp; design !&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;we need P2M2P&amp;nbsp; mode for this...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//////////////////////////////////////////////////&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am confused,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;it was simply done in old AT91SAM7X256 ....&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//////////////////////////////////////////////////&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;AT91SAM7X256: DOC6120&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;22. Peripheral DMA Controller (PDC)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;22.1 Overview&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The Peripheral DMA Controller (PDC) transfers data between on-chip serial peripherals such as&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the UART, USART, SSC, SPI, MCI and the on- and off-chip memories. Using the Peripheral&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DMA Controller avoids processor intervention and removes the processor interrupt-handling&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;overhead. This significantly reduces the number of clock cycles required for a data transfer and,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;as a result, improves the performance of the microcontroller and makes it more power efficient.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;============&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The PDC channels are implemented in pairs, each pair being dedicated to a particular peripheral.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;=============================== THIS IS FULL DUPLEX ======================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;One channel in the pair is dedicated to the receiving channel and one to the transmitting&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;channel of each UART, USART, SSC and SPI.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;==========================================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The user interface of a PDC channel is integrated in the memory space of each peripheral. It&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;contains:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;• A 32-bit memory pointer register&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;• A 16-bit transfer count register&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;• A 32-bit register for next memory pointer&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;• A 16-bit register for next transfer count&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The peripheral triggers PDC transfers using transmit and receive signals. When the programmed&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;data&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;==============================================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;it seems that :&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;the GPDMA cannot handle full duplex in SSP/SPI&amp;nbsp; ( sending 1024 bytes array and receiving 1024 bytes array simultaneously )&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;and I have to build it without GPDMA and by byte transfer interrupts &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"10 times per second each 1024 bytes" = 10240 interrupts will be over head to &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;my full featured heavy and complicated design,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;================================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;any comment ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;am I wrong ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:55:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-GPDMA-SSP-Burst-size-memory-boundary-alignment/m-p/522531#M5167</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:55:37Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 + GPDMA + SSP + Burst size + memory boundary/alignment</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-GPDMA-SSP-Burst-size-memory-boundary-alignment/m-p/522532#M5168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by solsal on Sat Aug 25 23:44:36 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;SSP INTERRUPTS ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Table 376: SSPn Raw Interrupt Status register (SSP0RIS - address 0x4008 8018, SSP1RIS -0x4003 0018) bit description&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Bit&amp;nbsp; Symbol&amp;nbsp;&amp;nbsp;&amp;nbsp; Description&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ResetValue&amp;nbsp; Comment&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;0&amp;nbsp;&amp;nbsp;&amp;nbsp; RORRIS&amp;nbsp;&amp;nbsp;&amp;nbsp; This bit is 1 if another frame was completely received while the RxFIFO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; error &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; was full. The ARM spec implies that the preceding frame data is&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; status&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; overwritten by the new frame data when this occurs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1&amp;nbsp;&amp;nbsp;&amp;nbsp; RTRIS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; This bit is 1 if the Rx FIFO is not empty, and has not been read for a&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; error&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "timeout period". The timeout period is the same for master and slave&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; status&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; modes and is determined by the SSP bit rate: 32 bits at PCLK /&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (CPSDVSR × [SCR+1]).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2&amp;nbsp;&amp;nbsp;&amp;nbsp; RXRIS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; This bit is 1 if the Rx FIFO is at least half full.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; read RX fifo&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3&amp;nbsp;&amp;nbsp;&amp;nbsp; TXRIS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; This bit is 1 if the Tx FIFO is at least half empty.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; write to TX fifo&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; till end of stream&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;31:4 - Reserved, user software should not write ones to reserved bits. The&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NA&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; value read from a reserved bit is not defined.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;=========================================================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;how can we use these interrupts bits for a full_duplex byte_by_byte transfer in LPC1768 SSP(SPI) peripheral ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;=========================================================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;example problem:( send and receive some bytes (1-by-1) by SSP , using interrupt&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. I want to do this by interrupt mode , ( NO Polling the SR register , because of software overhead )&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. for receiving 1 byte from SSP ,I send 1 byte to SSP , then.... by which interrupt condition I will be warned &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; that the receive or send byte is reached(done) ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:55:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-GPDMA-SSP-Burst-size-memory-boundary-alignment/m-p/522532#M5168</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:55:38Z</dc:date>
    </item>
  </channel>
</rss>