<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC11xx ADC in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11xx-ADC/m-p/522529#M5165</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanB on Sat Feb 13 10:20:31 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have an application where the ADC is set to runs continuously. It reads 6 channels, 10 bits per channel, with a division ratio of 56. With a 48MHz clock the sequence repeats 13000 times a second.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The interrupt is triggered by the end of the conversion on AD7, and the routine reads all the data registers (not the global data register - I have read the errata)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Although the data seem correct, every channel has bit 30 set indicating an overrun.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I even reduced the interrupt service routine so that it did no more than read the data registers and toggle a GPIO port.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I could see on the 'scope that it was running 13000 times a second, but it still indicated overruns on each channel.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Should I just ignore bit 30? Or has there really been an overrun?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:39:20 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:39:20Z</dc:date>
    <item>
      <title>LPC11xx ADC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11xx-ADC/m-p/522529#M5165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanB on Sat Feb 13 10:20:31 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have an application where the ADC is set to runs continuously. It reads 6 channels, 10 bits per channel, with a division ratio of 56. With a 48MHz clock the sequence repeats 13000 times a second.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The interrupt is triggered by the end of the conversion on AD7, and the routine reads all the data registers (not the global data register - I have read the errata)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Although the data seem correct, every channel has bit 30 set indicating an overrun.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I even reduced the interrupt service routine so that it did no more than read the data registers and toggle a GPIO port.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I could see on the 'scope that it was running 13000 times a second, but it still indicated overruns on each channel.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Should I just ignore bit 30? Or has there really been an overrun?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:39:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11xx-ADC/m-p/522529#M5165</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:39:20Z</dc:date>
    </item>
  </channel>
</rss>