<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Pinout for MCU-Link Pro to LPC832 in CMSIS-DAP debugging</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-for-MCU-Link-Pro-to-LPC832-in-CMSIS-DAP-debugging/m-p/1598639#M51627</link>
    <description>&lt;P&gt;Hi.&amp;nbsp; I'm using a free-standing LPC832 - not part of any EVK - and the SWD connections as referenced in *1 work fine if I'm using the J-Link debugger.&amp;nbsp; However, if I debug with LinkServer and the MCU-Link Pro, with the same pin connections, I get the following:&lt;/P&gt;&lt;PRE&gt;02: Failed on Connect&lt;BR /&gt;Target marked as not debuggable.&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset&lt;BR /&gt;Remote communication error. Target disconnected.: Connection reset by peer.&lt;/PRE&gt;&lt;P&gt;Does the stand-alone LPC832 not support CMSIS-DAP debugging?&amp;nbsp; Are my pins connected incorrectly?&amp;nbsp; I could flash the MCU-Link Pro with Segger firmware and use it as another J-Link debug probe, but I'd rather have two types of probes.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;*1:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-and-debugger-configuration-for-reliable-SWD-on-LPC810/m-p/693794" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-and-debugger-configuration-for-reliable-SWD-on-LPC810/m-p/693794&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 14 Feb 2023 07:02:51 GMT</pubDate>
    <dc:creator>aaronm</dc:creator>
    <dc:date>2023-02-14T07:02:51Z</dc:date>
    <item>
      <title>Pinout for MCU-Link Pro to LPC832 in CMSIS-DAP debugging</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-for-MCU-Link-Pro-to-LPC832-in-CMSIS-DAP-debugging/m-p/1598639#M51627</link>
      <description>&lt;P&gt;Hi.&amp;nbsp; I'm using a free-standing LPC832 - not part of any EVK - and the SWD connections as referenced in *1 work fine if I'm using the J-Link debugger.&amp;nbsp; However, if I debug with LinkServer and the MCU-Link Pro, with the same pin connections, I get the following:&lt;/P&gt;&lt;PRE&gt;02: Failed on Connect&lt;BR /&gt;Target marked as not debuggable.&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset&lt;BR /&gt;Remote communication error. Target disconnected.: Connection reset by peer.&lt;/PRE&gt;&lt;P&gt;Does the stand-alone LPC832 not support CMSIS-DAP debugging?&amp;nbsp; Are my pins connected incorrectly?&amp;nbsp; I could flash the MCU-Link Pro with Segger firmware and use it as another J-Link debug probe, but I'd rather have two types of probes.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;*1:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-and-debugger-configuration-for-reliable-SWD-on-LPC810/m-p/693794" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-and-debugger-configuration-for-reliable-SWD-on-LPC810/m-p/693794&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Feb 2023 07:02:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-for-MCU-Link-Pro-to-LPC832-in-CMSIS-DAP-debugging/m-p/1598639#M51627</guid>
      <dc:creator>aaronm</dc:creator>
      <dc:date>2023-02-14T07:02:51Z</dc:date>
    </item>
    <item>
      <title>Re: Pinout for MCU-Link Pro to LPC832 in CMSIS-DAP debugging</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-for-MCU-Link-Pro-to-LPC832-in-CMSIS-DAP-debugging/m-p/1598687#M51629</link>
      <description>&lt;P&gt;Some debug probes have configurable options to enable/disable the 3.3V supply to the target through the debug adapter.&lt;BR /&gt;Perhaps this is your problem ?&lt;/P&gt;</description>
      <pubDate>Tue, 14 Feb 2023 07:58:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-for-MCU-Link-Pro-to-LPC832-in-CMSIS-DAP-debugging/m-p/1598687#M51629</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2023-02-14T07:58:22Z</dc:date>
    </item>
    <item>
      <title>Re: Pinout for MCU-Link Pro to LPC832 in CMSIS-DAP debugging</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-for-MCU-Link-Pro-to-LPC832-in-CMSIS-DAP-debugging/m-p/1599140#M51634</link>
      <description>&lt;P&gt;I figured it out: the TDO pin needs to be connected for CMSIS-DAP debugging.&amp;nbsp; Evidently, this is not necessary with J-Link debugging - as I've experienced in actual practice.&amp;nbsp; The MCU-LINK Pro schematic helped.&amp;nbsp; See page 4, "&lt;SPAN&gt;Cortex Debug (SWD/JTAG) interface."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/downloads/en/schematics/MCU-LINK-SCH.pdf" target="_blank"&gt;https://www.nxp.com/downloads/en/schematics/MCU-LINK-SCH.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Feb 2023 23:52:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-for-MCU-Link-Pro-to-LPC832-in-CMSIS-DAP-debugging/m-p/1599140#M51634</guid>
      <dc:creator>aaronm</dc:creator>
      <dc:date>2023-02-14T23:52:35Z</dc:date>
    </item>
    <item>
      <title>Re: Pinout for MCU-Link Pro to LPC832 in CMSIS-DAP debugging</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-for-MCU-Link-Pro-to-LPC832-in-CMSIS-DAP-debugging/m-p/1599146#M51635</link>
      <description>&lt;P&gt;Good point, but MCU-Link (base model) cant power a target. MCU-Link Pro can.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 00:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pinout-for-MCU-Link-Pro-to-LPC832-in-CMSIS-DAP-debugging/m-p/1599146#M51635</guid>
      <dc:creator>brendonslade</dc:creator>
      <dc:date>2023-02-15T00:30:50Z</dc:date>
    </item>
  </channel>
</rss>