<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SHA 256 Calculation LPC55S28 - BUG in fsl_hascrypt.c ? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SHA-256-Calculation-LPC55S28-BUG-in-fsl-hascrypt-c/m-p/1596270#M51579</link>
    <description>&lt;P&gt;I have a few questions about the SHA function and the implementation in the FSL drivers fsl_hashcrypt.c.&lt;/P&gt;&lt;P&gt;I need the SHA checksum to check the firmware in the internal flash memory&lt;/P&gt;&lt;P&gt;I am currently using version 11 of the LPC55S28 SDK and the HASHCRYPT_SHA() function there&lt;/P&gt;&lt;P&gt;1. Is it possible to use a flash memory area directly as a source in register MEMADDR, according to the LPC manual only SRAM0 or SRAMX can be used, but the version with direct flash access is also suggested here in the forum, or does the flash data have to be copied to the RAM first? .&lt;/P&gt;&lt;P&gt;The calculation with the flash memory actually worked without any problems and also generated correct SHA checksums.&lt;/P&gt;&lt;P&gt;2. There seems to be a bug in the FSL drivers in the fsl_hashcrypt.c module. The functions of the SHA calculation, e.g. hashcrypt_sha_process_message_data, only evaluate the HASHCRYPT_STATUS_DIGEST_MASK but not HASHCRYPT_STATUS_ERROR_MASK in the event of an error, the drivers never come back and the watchdog strikes. This happens when trying to calculate the SHA of a deleted Flashpage, where the HASHCRYPT_STATUS_ERROR_MASK flag is set.&lt;/P&gt;&lt;P&gt;We are currently using the SDK version 11, but the query is also identical in version 12. The start address of the flash memory is aligned. (0x20000)&lt;/P&gt;&lt;P&gt;3. The SHA drivers do not check the length of the data, if more than the possible 2047 blocks 131008 bytes are specified, there is no error message but an incorrect SHA&lt;/P&gt;&lt;P&gt;It would be great if someone could help me with the issues.&lt;/P&gt;</description>
    <pubDate>Thu, 09 Feb 2023 06:45:25 GMT</pubDate>
    <dc:creator>Baur_phg</dc:creator>
    <dc:date>2023-02-09T06:45:25Z</dc:date>
    <item>
      <title>SHA 256 Calculation LPC55S28 - BUG in fsl_hascrypt.c ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SHA-256-Calculation-LPC55S28-BUG-in-fsl-hascrypt-c/m-p/1596270#M51579</link>
      <description>&lt;P&gt;I have a few questions about the SHA function and the implementation in the FSL drivers fsl_hashcrypt.c.&lt;/P&gt;&lt;P&gt;I need the SHA checksum to check the firmware in the internal flash memory&lt;/P&gt;&lt;P&gt;I am currently using version 11 of the LPC55S28 SDK and the HASHCRYPT_SHA() function there&lt;/P&gt;&lt;P&gt;1. Is it possible to use a flash memory area directly as a source in register MEMADDR, according to the LPC manual only SRAM0 or SRAMX can be used, but the version with direct flash access is also suggested here in the forum, or does the flash data have to be copied to the RAM first? .&lt;/P&gt;&lt;P&gt;The calculation with the flash memory actually worked without any problems and also generated correct SHA checksums.&lt;/P&gt;&lt;P&gt;2. There seems to be a bug in the FSL drivers in the fsl_hashcrypt.c module. The functions of the SHA calculation, e.g. hashcrypt_sha_process_message_data, only evaluate the HASHCRYPT_STATUS_DIGEST_MASK but not HASHCRYPT_STATUS_ERROR_MASK in the event of an error, the drivers never come back and the watchdog strikes. This happens when trying to calculate the SHA of a deleted Flashpage, where the HASHCRYPT_STATUS_ERROR_MASK flag is set.&lt;/P&gt;&lt;P&gt;We are currently using the SDK version 11, but the query is also identical in version 12. The start address of the flash memory is aligned. (0x20000)&lt;/P&gt;&lt;P&gt;3. The SHA drivers do not check the length of the data, if more than the possible 2047 blocks 131008 bytes are specified, there is no error message but an incorrect SHA&lt;/P&gt;&lt;P&gt;It would be great if someone could help me with the issues.&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 06:45:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SHA-256-Calculation-LPC55S28-BUG-in-fsl-hascrypt-c/m-p/1596270#M51579</guid>
      <dc:creator>Baur_phg</dc:creator>
      <dc:date>2023-02-09T06:45:25Z</dc:date>
    </item>
    <item>
      <title>Re: SHA 256 Calculation LPC55S28 - BUG in fsl_hascrypt.c ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SHA-256-Calculation-LPC55S28-BUG-in-fsl-hascrypt-c/m-p/1597867#M51610</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I have asked AE&amp;nbsp; security team, I will answer your question after I get feedback.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 13 Feb 2023 05:55:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SHA-256-Calculation-LPC55S28-BUG-in-fsl-hascrypt-c/m-p/1597867#M51610</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-02-13T05:55:30Z</dc:date>
    </item>
    <item>
      <title>Re: SHA 256 Calculation LPC55S28 - BUG in fsl_hascrypt.c ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SHA-256-Calculation-LPC55S28-BUG-in-fsl-hascrypt-c/m-p/1600340#M51653</link>
      <description>&lt;P&gt;Hi, Baur&lt;/P&gt;&lt;P&gt;Can you tell us the target application? The item is required by the AE team.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 16 Feb 2023 08:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SHA-256-Calculation-LPC55S28-BUG-in-fsl-hascrypt-c/m-p/1600340#M51653</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-02-16T08:55:52Z</dc:date>
    </item>
    <item>
      <title>Re: SHA 256 Calculation LPC55S28 - BUG in fsl_hascrypt.c ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SHA-256-Calculation-LPC55S28-BUG-in-fsl-hascrypt-c/m-p/1600813#M51660</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This is the feedback from AE engineer:&lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;
&lt;P&gt;As stated in UM, SHA engine can read from SRAM or flash.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1676602560229.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/211308i953C2F9D57DDA9F3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1676602560229.png" alt="xiangjun_rong_0-1676602560229.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1676602560229.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2. The root cause is LPC5500 flash cannot be read after erase operation. I have created a ticket to SDK team to improve this issue.&lt;/P&gt;
&lt;P&gt;3. This is a SDK issue, the SDK driver doesn't check the length of the content. I have created a SDK ticket for the issue.&lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 03:01:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SHA-256-Calculation-LPC55S28-BUG-in-fsl-hascrypt-c/m-p/1600813#M51660</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-02-17T03:01:54Z</dc:date>
    </item>
    <item>
      <title>Re: SHA 256 Calculation LPC55S28 - BUG in fsl_hascrypt.c ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SHA-256-Calculation-LPC55S28-BUG-in-fsl-hascrypt-c/m-p/1604458#M51703</link>
      <description>&lt;P&gt;Thanks for the answer and the help,&lt;/P&gt;&lt;P&gt;In the UM register description of the memory address register MEMADDR, only the SRAM is specified, thats why i was a little bit confused&lt;/P&gt;&lt;P&gt;I modified the sha function and check the HW Error Flag, now it returns with Error Status if the Flash is not programmed.&lt;/P&gt;&lt;P&gt;now it works as expected&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 23 Feb 2023 09:10:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SHA-256-Calculation-LPC55S28-BUG-in-fsl-hascrypt-c/m-p/1604458#M51703</guid>
      <dc:creator>Baur_phg</dc:creator>
      <dc:date>2023-02-23T09:10:18Z</dc:date>
    </item>
  </channel>
</rss>