<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC11E6x Boot Behavior PIO0_3</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E6x-Boot-Behavior-PIO0-3/m-p/1592654#M51511</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;LPC11E6x enters ISP mode when PIO0_1 is sampled low after reset, assuming no watchdog flag or CRP.&amp;nbsp; After this determination, is there any dependency on PIO0_3 to decide what happens next, or does it enter UART ISP directly?&lt;/P&gt;&lt;P&gt;The User Manual states there is no USB boot facility on LPC11E6x but there is a flow chart Figure 86 which does not clearly state what happens based on the status of the USB ISP pin PIO0_3.&lt;/P&gt;&lt;P&gt;I need PIO0_3 for something else and cannot guarantee it would always be low on boot.&lt;/P&gt;&lt;P&gt;MikeN&lt;/P&gt;</description>
    <pubDate>Thu, 02 Feb 2023 23:01:41 GMT</pubDate>
    <dc:creator>mikenn</dc:creator>
    <dc:date>2023-02-02T23:01:41Z</dc:date>
    <item>
      <title>LPC11E6x Boot Behavior PIO0_3</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E6x-Boot-Behavior-PIO0-3/m-p/1592654#M51511</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;LPC11E6x enters ISP mode when PIO0_1 is sampled low after reset, assuming no watchdog flag or CRP.&amp;nbsp; After this determination, is there any dependency on PIO0_3 to decide what happens next, or does it enter UART ISP directly?&lt;/P&gt;&lt;P&gt;The User Manual states there is no USB boot facility on LPC11E6x but there is a flow chart Figure 86 which does not clearly state what happens based on the status of the USB ISP pin PIO0_3.&lt;/P&gt;&lt;P&gt;I need PIO0_3 for something else and cannot guarantee it would always be low on boot.&lt;/P&gt;&lt;P&gt;MikeN&lt;/P&gt;</description>
      <pubDate>Thu, 02 Feb 2023 23:01:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E6x-Boot-Behavior-PIO0-3/m-p/1592654#M51511</guid>
      <dc:creator>mikenn</dc:creator>
      <dc:date>2023-02-02T23:01:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11E6x Boot Behavior PIO0_3</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E6x-Boot-Behavior-PIO0-3/m-p/1592707#M51512</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the LPC11E6x does not have USB port, it can not boot application code from USB port. The PIO0_1 pin is the only pin to be sampled during/after Reset to determine if boot mode is entered and boot from uart0 pins or application code is executed from flash.&lt;/P&gt;
&lt;P&gt;The PIO0_3 is NOT sampled during/after Reset for LPC11E6x, you can use PIO0_3 pin as general GPIO pin.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 03 Feb 2023 01:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E6x-Boot-Behavior-PIO0-3/m-p/1592707#M51512</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-02-03T01:39:45Z</dc:date>
    </item>
  </channel>
</rss>