<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S16 64-pin Processor Verification in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-64-pin-Processor-Verification/m-p/1592629#M51510</link>
    <description>&lt;P&gt;Thanks for the response,&lt;/P&gt;&lt;P&gt;Those voltages are reading correctly but I am still unable to read a signature from the device and RESETN and ISP is pulled high.&lt;/P&gt;&lt;P&gt;A little more information:&lt;/P&gt;&lt;P&gt;Serial cable connects through a level shifter when reading the EVK device from JP3 Serial Port. My understanding is that this is the USART0. On the 64-pin, I am connecting to P0_29,30 for RX and TX respectively.&lt;/P&gt;&lt;P&gt;Port0_5 is ISP&lt;/P&gt;&lt;P&gt;Pulling ISP low and resetting (pulling RESETN low) should put it in ISP mode and default these pins to their ISP mode condition, but I don't get any response from the device read.&lt;/P&gt;</description>
    <pubDate>Thu, 02 Feb 2023 21:10:47 GMT</pubDate>
    <dc:creator>Matthias9265</dc:creator>
    <dc:date>2023-02-02T21:10:47Z</dc:date>
    <item>
      <title>LPC55S16 64-pin Processor Verification</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-64-pin-Processor-Verification/m-p/1590831#M51470</link>
      <description>&lt;P&gt;Hi All!&lt;/P&gt;&lt;P&gt;I'm developing a board using the LPC55S16JBD64E and I've run into some issues with validating the device is powered up. Does anyone have a particular examples or insight of methods to verify the processor is successfully powered?&lt;/P&gt;&lt;P&gt;I've used the EVK and read its device signature using Flash Magic through USART using a serial-USB cable. If my understanding is correct, this should be a valid method, but so far unsuccessful.&lt;/P&gt;&lt;P&gt;The signal coming out of pin 31 (LX) appears correct on the scope (similar to the output on the EVK).&lt;/P&gt;&lt;P&gt;Both Oscillators are running as well.&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 22:42:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-64-pin-Processor-Verification/m-p/1590831#M51470</guid>
      <dc:creator>Matthias9265</dc:creator>
      <dc:date>2023-01-31T22:42:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 64-pin Processor Verification</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-64-pin-Processor-Verification/m-p/1592153#M51497</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211485"&gt;@Matthias9265&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;You can measure the voltage from below two detection points：&lt;/P&gt;
&lt;P&gt;Point 1 is input, should 1.8-3.6V, usually 3.3v.&lt;/P&gt;
&lt;P&gt;Point 2 is output of DCDC, should 1.1V.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1675327423581.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209330iFE76DB05D7984C8A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1675327423581.png" alt="Alice_Yang_0-1675327423581.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Feb 2023 08:46:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-64-pin-Processor-Verification/m-p/1592153#M51497</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-02-02T08:46:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 64-pin Processor Verification</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-64-pin-Processor-Verification/m-p/1592629#M51510</link>
      <description>&lt;P&gt;Thanks for the response,&lt;/P&gt;&lt;P&gt;Those voltages are reading correctly but I am still unable to read a signature from the device and RESETN and ISP is pulled high.&lt;/P&gt;&lt;P&gt;A little more information:&lt;/P&gt;&lt;P&gt;Serial cable connects through a level shifter when reading the EVK device from JP3 Serial Port. My understanding is that this is the USART0. On the 64-pin, I am connecting to P0_29,30 for RX and TX respectively.&lt;/P&gt;&lt;P&gt;Port0_5 is ISP&lt;/P&gt;&lt;P&gt;Pulling ISP low and resetting (pulling RESETN low) should put it in ISP mode and default these pins to their ISP mode condition, but I don't get any response from the device read.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Feb 2023 21:10:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-64-pin-Processor-Verification/m-p/1592629#M51510</guid>
      <dc:creator>Matthias9265</dc:creator>
      <dc:date>2023-02-02T21:10:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 64-pin Processor Verification</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-64-pin-Processor-Verification/m-p/1593758#M51534</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211485"&gt;@Matthias9265&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;When in ISP mode,&amp;nbsp;&lt;SPAN&gt;P0_29 as UART0_RX,&amp;nbsp;P0_30 as UART0_TX, so connect the TX of your USB-UART transfer to P0_29 of your chip, and RX to P0_30.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 08:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-64-pin-Processor-Verification/m-p/1593758#M51534</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-02-06T08:11:53Z</dc:date>
    </item>
  </channel>
</rss>