<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: PLL0 input frequency range</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/PLL0-input-frequency-range/m-p/522509#M5145</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Tue Oct 08 22:54:10 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thomas,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I started out by stating that you should re-read the datasheet and user manual but it seems NXP messed up on this one.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The description on chapter 7.33.2 of the datasheet (LPC178X_7X.pdf) states that the main oscillator needs a crystal in the range of 10-25 MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But then, in 14.2 there is something else ... ranges run from 1 up to 25 MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The same is also written in 11.3 (Dynamic characteristics).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You are not using the oscillator in slave mode (according to fig. 36 in chapter 14.2) with a 4 MHz oscillator which is perfectly within spec.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So nothing to worry about.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob - NXP definitely made this a tricky one to answer ;)&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:54:37 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:54:37Z</dc:date>
    <item>
      <title>PLL0 input frequency range</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PLL0-input-frequency-range/m-p/522508#M5144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Dragonheart77 on Sat Oct 05 00:16:57 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi there,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I use the lpc1778 and the input frequency range for the PLL0 of the LPC17xx family is not clear to me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The data sheet just tells me about a range of 10 to 25 MHz for PLL1. There is no such statement for PLL0. It just says "are functionally &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;identical but have somewhat different input possibilities and output connections". Is it the same input frequency range for PLL0 like PLL1?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;For PPL1, mainly used for the USB clock, it sounds reasonable to allow 10 to 25 MHz and save something in the PLL block and silicon. Otherwise 2 different PLL blocks in silicon? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Also the source code of the "system_LPC177x_8x.c" says "F_in is in the range of 1 MHz to 25 MHz" as comment. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Currently I use an external 4 MHz oscillator. M = 30, P = 1 -&amp;gt; PLL Clk Out = 120 MHz, Fcco = 240 MHz OK. It works on 4 boards so far.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But does it always work in the temperature range?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I need the 4 MHz for other devices on my board and so I want to save parts and money. I'm not sure if the 4 MHz input is valid or not.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thomas&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:54:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PLL0-input-frequency-range/m-p/522508#M5144</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:54:36Z</dc:date>
    </item>
    <item>
      <title>Re: PLL0 input frequency range</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PLL0-input-frequency-range/m-p/522509#M5145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Tue Oct 08 22:54:10 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thomas,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I started out by stating that you should re-read the datasheet and user manual but it seems NXP messed up on this one.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The description on chapter 7.33.2 of the datasheet (LPC178X_7X.pdf) states that the main oscillator needs a crystal in the range of 10-25 MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But then, in 14.2 there is something else ... ranges run from 1 up to 25 MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The same is also written in 11.3 (Dynamic characteristics).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You are not using the oscillator in slave mode (according to fig. 36 in chapter 14.2) with a 4 MHz oscillator which is perfectly within spec.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So nothing to worry about.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob - NXP definitely made this a tricky one to answer ;)&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:54:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PLL0-input-frequency-range/m-p/522509#M5145</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:54:37Z</dc:date>
    </item>
  </channel>
</rss>