<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC 1788 with SC18IS606 I2C communication in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1788-with-SC18IS606-I2C-communication/m-p/1588997#M51418</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to use LPC1788 OEM board together with SC18IS606 circuit via I2C bus.&lt;/P&gt;&lt;P&gt;For I2C bus i am using LPCOPEN drivers, the latest version. Also, in my application i am using LWIP stack for an ethernet communication and an UART connection. These other two communication types are working fine, but i have an issue on I2C bus.&lt;/P&gt;&lt;P&gt;I2C signals are connected to pin 108 (I2C0_SCL) and pin 109 (I2C0_SDA) from OEM board. In application i setup these signals to P5[2] and P5[3] with IOCON_FUNC5 and I initialized I2C0 to work in polling mode with 100 kHz speed. I2C slave address is 0x50.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My issue is that after i send a first command to SC18IS606, SDA and SCL goes to LOW and I can not send another command on I2C bus. I can not figure out what is happening because I used in past the same LPC1788 OEM board and I2C LPCOpen drivers with another circuit, TMP422 and everything worked fine.&lt;/P&gt;&lt;P&gt;After I2C is initialized, I wrote to SC18IS606 to send me the version (0xFE function id), but after the command is sent, I2C bus is stuck.&lt;/P&gt;&lt;P&gt;Of course I want to use this circuit for I2C to SPI bridge. But after first command (does not matter what command is sent - SPI configuration, Idle command, Read version command), SDA and SCL goes to LOW state even if I have pullup rezistor on these lines.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Denisa&lt;/P&gt;</description>
    <pubDate>Fri, 27 Jan 2023 16:46:38 GMT</pubDate>
    <dc:creator>dimoftedenisa</dc:creator>
    <dc:date>2023-01-27T16:46:38Z</dc:date>
    <item>
      <title>LPC 1788 with SC18IS606 I2C communication</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1788-with-SC18IS606-I2C-communication/m-p/1588997#M51418</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to use LPC1788 OEM board together with SC18IS606 circuit via I2C bus.&lt;/P&gt;&lt;P&gt;For I2C bus i am using LPCOPEN drivers, the latest version. Also, in my application i am using LWIP stack for an ethernet communication and an UART connection. These other two communication types are working fine, but i have an issue on I2C bus.&lt;/P&gt;&lt;P&gt;I2C signals are connected to pin 108 (I2C0_SCL) and pin 109 (I2C0_SDA) from OEM board. In application i setup these signals to P5[2] and P5[3] with IOCON_FUNC5 and I initialized I2C0 to work in polling mode with 100 kHz speed. I2C slave address is 0x50.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My issue is that after i send a first command to SC18IS606, SDA and SCL goes to LOW and I can not send another command on I2C bus. I can not figure out what is happening because I used in past the same LPC1788 OEM board and I2C LPCOpen drivers with another circuit, TMP422 and everything worked fine.&lt;/P&gt;&lt;P&gt;After I2C is initialized, I wrote to SC18IS606 to send me the version (0xFE function id), but after the command is sent, I2C bus is stuck.&lt;/P&gt;&lt;P&gt;Of course I want to use this circuit for I2C to SPI bridge. But after first command (does not matter what command is sent - SPI configuration, Idle command, Read version command), SDA and SCL goes to LOW state even if I have pullup rezistor on these lines.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Denisa&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jan 2023 16:46:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1788-with-SC18IS606-I2C-communication/m-p/1588997#M51418</guid>
      <dc:creator>dimoftedenisa</dc:creator>
      <dc:date>2023-01-27T16:46:38Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 1788 with SC18IS606 I2C communication</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1788-with-SC18IS606-I2C-communication/m-p/1590362#M51458</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/153826"&gt;@dimoftedenisa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Recommend you first use a project only includes I2C, without&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;ethernet communication and an UART connection. Then check&amp;nbsp;SC18IS606 datasheet,&amp;nbsp; &amp;nbsp;use logic analyzer measures the signal, whether it meet the signal sequence DS mentioned.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 07:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1788-with-SC18IS606-I2C-communication/m-p/1590362#M51458</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-01-31T07:38:27Z</dc:date>
    </item>
  </channel>
</rss>