<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC51U68 HR PWM in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-HR-PWM/m-p/1587282#M51363</link>
    <description>&lt;P&gt;I'm looking at the LPC51U68 series of MCUs and an alternative to another MCU that has a High-Resolution PWM.&amp;nbsp; This is a new MCU for me, and I haven't use an NXP MCU for about 5 years now.&amp;nbsp; I'm struggling to find information on the PWM output of the LPC51U68 (it's likely in the datasheet but I can't seem to find what I'm looking for).&amp;nbsp; Is there some documentation on setting up the timing?&amp;nbsp; What I want to know.&amp;nbsp; Making the math easy (assuming it is right) if the sys clock is 100MHz, and PWM period to 1us, then there are 100 quantized PWM steps.&amp;nbsp; Is there any way to increase the number of quantized steps, say 10x, or am I stuck with the sys clock for max resolution?&lt;/P&gt;</description>
    <pubDate>Tue, 24 Jan 2023 17:56:37 GMT</pubDate>
    <dc:creator>xcellsior</dc:creator>
    <dc:date>2023-01-24T17:56:37Z</dc:date>
    <item>
      <title>LPC51U68 HR PWM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-HR-PWM/m-p/1587282#M51363</link>
      <description>&lt;P&gt;I'm looking at the LPC51U68 series of MCUs and an alternative to another MCU that has a High-Resolution PWM.&amp;nbsp; This is a new MCU for me, and I haven't use an NXP MCU for about 5 years now.&amp;nbsp; I'm struggling to find information on the PWM output of the LPC51U68 (it's likely in the datasheet but I can't seem to find what I'm looking for).&amp;nbsp; Is there some documentation on setting up the timing?&amp;nbsp; What I want to know.&amp;nbsp; Making the math easy (assuming it is right) if the sys clock is 100MHz, and PWM period to 1us, then there are 100 quantized PWM steps.&amp;nbsp; Is there any way to increase the number of quantized steps, say 10x, or am I stuck with the sys clock for max resolution?&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jan 2023 17:56:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-HR-PWM/m-p/1587282#M51363</guid>
      <dc:creator>xcellsior</dc:creator>
      <dc:date>2023-01-24T17:56:37Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 HR PWM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-HR-PWM/m-p/1590773#M51467</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;If you refer to the SCTimer/PWM of the LPC51U68, you can find more information about it in the &lt;A href="https://www.nxp.com/webapp/Download?colCode=UM11071" target="_blank" rel="noopener"&gt;LPC51U68 User Manual&lt;/A&gt;, also for more detail there is the &lt;A href="https://www.nxp.com/docs/en/application-note/AN11538.zip" target="_blank" rel="noopener"&gt;SCTimer/PWM cookbook&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;An alternative is the &lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/kv-series-arm-cortex-m4-m0-plus-m7/kinetis-kv4x-168-mhz-high-performance-motor-power-conversion-mcus-based-on-arm-cortex-m4:KV4x" target="_blank" rel="noopener"&gt;KV4x&lt;/A&gt;, which features PWMA/eFlexPWM peripheral with NanoEdge high resolution. For more information on this, you can refer to the &lt;A href="https://www.nxp.com/webapp/Download?colCode=KV4XP100M168RM" target="_blank" rel="noopener"&gt;reference manual&lt;/A&gt; and the post &lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Nano-edge-placement-feature-for-eFlexPWM-module-based-on-KV4x/ta-p/1105571" target="_blank" rel="noopener"&gt;Nano-edge placement feature for eFlexPWM module based on KV4x&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 19:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-HR-PWM/m-p/1590773#M51467</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-01-31T19:14:19Z</dc:date>
    </item>
  </channel>
</rss>