<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can the SCT on an LPC5502 be used for reading a rotary encoder? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-SCT-on-an-LPC5502-be-used-for-reading-a-rotary-encoder/m-p/1585359#M51324</link>
    <description>&lt;P&gt;We are currently using the LPC1752 in a number of devices. As this chip is approaching an End-of-Lifetime condition, and I have to redesign one of the devices, I found the LPC5502 as a potential replacement. It is just lacking one device: A way to decode a simple rotary encoder switch.&lt;/P&gt;&lt;P&gt;Is it possible to emulate the LPC1752 QEI (Quadrature Encoder Interface) with the LPC5502 SCT? With the ability to create a state machine it looks like it, but the documentation in the user manual is more than confusing, and the SCT tool is no real help, either.&lt;/P&gt;</description>
    <pubDate>Thu, 19 Jan 2023 10:39:25 GMT</pubDate>
    <dc:creator>Treczoks</dc:creator>
    <dc:date>2023-01-19T10:39:25Z</dc:date>
    <item>
      <title>Can the SCT on an LPC5502 be used for reading a rotary encoder?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-SCT-on-an-LPC5502-be-used-for-reading-a-rotary-encoder/m-p/1585359#M51324</link>
      <description>&lt;P&gt;We are currently using the LPC1752 in a number of devices. As this chip is approaching an End-of-Lifetime condition, and I have to redesign one of the devices, I found the LPC5502 as a potential replacement. It is just lacking one device: A way to decode a simple rotary encoder switch.&lt;/P&gt;&lt;P&gt;Is it possible to emulate the LPC1752 QEI (Quadrature Encoder Interface) with the LPC5502 SCT? With the ability to create a state machine it looks like it, but the documentation in the user manual is more than confusing, and the SCT tool is no real help, either.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jan 2023 10:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-SCT-on-an-LPC5502-be-used-for-reading-a-rotary-encoder/m-p/1585359#M51324</guid>
      <dc:creator>Treczoks</dc:creator>
      <dc:date>2023-01-19T10:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: Can the SCT on an LPC5502 be used for reading a rotary encoder?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-SCT-on-an-LPC5502-be-used-for-reading-a-rotary-encoder/m-p/1586279#M51342</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;I'm sorry to inform you that we don't have any software example or documentation to reading a rotary encoder with the SCTimer/PWM module, so I can't tell you if it's possible. You would be the first person to implement it. If you do, I would appreciate your feedback.&lt;/P&gt;
&lt;P&gt;On the other hand, in addition to the manual reference, you can also refer to the &lt;A href="https://www.nxp.com/docs/en/application-note/AN11538.zip" target="_blank" rel="noopener"&gt;SCTimer/PWM cookbook&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jan 2023 22:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-SCT-on-an-LPC5502-be-used-for-reading-a-rotary-encoder/m-p/1586279#M51342</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-01-20T22:06:11Z</dc:date>
    </item>
  </channel>
</rss>