<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックMCU selection</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-selection/m-p/1583880#M51292</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm looking for MCU, that will be able to handle:&lt;/P&gt;&lt;P&gt;1) Read one 8 bit (or 2x 4 bit) 48 MHz data stream. Quad SPI is suitable for it, but any interface that can read 8 bit or 4 bit parallel data stream synchronized by 48 MHz clock is suitable.&lt;/P&gt;&lt;P&gt;2) External SDRAM memory interface&lt;/P&gt;&lt;P&gt;3) High speed USB interface.&lt;/P&gt;&lt;P&gt;4) At least 150 MHz CPU clock (not sure if it is enough).&lt;/P&gt;&lt;P&gt;The device will read incoming 8 bit (or 2x 4 bit) 48 MHz data stream, buffer it to SDRAM and another task will read buffered data from SDRAM, do some processing and send data via USB high speed.&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jan 2023 09:39:55 GMT</pubDate>
    <dc:creator>dusek_martin</dc:creator>
    <dc:date>2023-01-17T09:39:55Z</dc:date>
    <item>
      <title>MCU selection</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-selection/m-p/1583880#M51292</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm looking for MCU, that will be able to handle:&lt;/P&gt;&lt;P&gt;1) Read one 8 bit (or 2x 4 bit) 48 MHz data stream. Quad SPI is suitable for it, but any interface that can read 8 bit or 4 bit parallel data stream synchronized by 48 MHz clock is suitable.&lt;/P&gt;&lt;P&gt;2) External SDRAM memory interface&lt;/P&gt;&lt;P&gt;3) High speed USB interface.&lt;/P&gt;&lt;P&gt;4) At least 150 MHz CPU clock (not sure if it is enough).&lt;/P&gt;&lt;P&gt;The device will read incoming 8 bit (or 2x 4 bit) 48 MHz data stream, buffer it to SDRAM and another task will read buffered data from SDRAM, do some processing and send data via USB high speed.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 09:39:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-selection/m-p/1583880#M51292</guid>
      <dc:creator>dusek_martin</dc:creator>
      <dc:date>2023-01-17T09:39:55Z</dc:date>
    </item>
    <item>
      <title>Re: MCU selection</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-selection/m-p/1584604#M51308</link>
      <description>&lt;P&gt;Not really a MCU suggestion ...&lt;/P&gt;&lt;P&gt;I would focus on the serial input. An 48MHz synchronous clock is relatively high. SPI should cover it, but it still results in a significant throughput. You will very likely need DMA or a FIFO support.&lt;/P&gt;&lt;P&gt;Just having some experience with SD cards, clock rates beyond 25MHz require a proper PCB layout and bus termination, or you get physical signal problems.&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;EM&gt;&amp;gt; 2) External SDRAM memory interface&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would be careful with that. External memory is usually only 16-bit wide, making it significantly slower than internal RAM, and additionally causing internal bus contention with the throughput-demanding serial input.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would go for data package sizes not larger than 4 kB, thus the internal RAM of many M3 or M4 devices would suffice.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 12:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-selection/m-p/1584604#M51308</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2023-01-18T12:34:14Z</dc:date>
    </item>
  </channel>
</rss>