<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC82x Internal Voltage Ref to ADC?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-Internal-Voltage-Ref-to-ADC/m-p/1583611#M51287</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;(I thought I posted this question yesterday, but it seem to have disappeared. Weird.)&lt;/P&gt;&lt;P&gt;The LPC82x has an internal 0.9v voltage reference that the doc's state can be used as a reference input to the comparator peripheral.&lt;/P&gt;&lt;P&gt;Is it possible for this reference to be routed to an ADC input?&lt;/P&gt;&lt;P&gt;I ideally would like to be able to measure it with the ADC, so I can then determine the VREFP (and so VDD) voltages. I have done this with MKL03/05 in the past.&lt;/P&gt;&lt;P&gt;Thankyou!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jan 2023 03:18:47 GMT</pubDate>
    <dc:creator>mwp_nxp</dc:creator>
    <dc:date>2023-01-17T03:18:47Z</dc:date>
    <item>
      <title>LPC82x Internal Voltage Ref to ADC?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-Internal-Voltage-Ref-to-ADC/m-p/1583611#M51287</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;(I thought I posted this question yesterday, but it seem to have disappeared. Weird.)&lt;/P&gt;&lt;P&gt;The LPC82x has an internal 0.9v voltage reference that the doc's state can be used as a reference input to the comparator peripheral.&lt;/P&gt;&lt;P&gt;Is it possible for this reference to be routed to an ADC input?&lt;/P&gt;&lt;P&gt;I ideally would like to be able to measure it with the ADC, so I can then determine the VREFP (and so VDD) voltages. I have done this with MKL03/05 in the past.&lt;/P&gt;&lt;P&gt;Thankyou!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 03:18:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-Internal-Voltage-Ref-to-ADC/m-p/1583611#M51287</guid>
      <dc:creator>mwp_nxp</dc:creator>
      <dc:date>2023-01-17T03:18:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82x Internal Voltage Ref to ADC?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-Internal-Voltage-Ref-to-ADC/m-p/1584146#M51300</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/82499"&gt;@mwp_nxp&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Unfortunately, there is not an option for routing the 0.9V internal bandgap reference voltage to an ADC input channel for the LPC84x.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;As a recommendation, you could try reading the following Application Notes:&lt;/P&gt;
&lt;UL class="lia-align-justify" type="disc"&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5250.pdf" target="_self"&gt;AN5250. How to Increase the Analog-to-Digital Converter Accuracy in an Application&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4373.pdf" target="_self"&gt;AN4373. Cookbook for SAR ADC Measurements&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13102.pdf" target="_self"&gt;AN13102. How to Get Best ADC Accuracy for LPC800&lt;/A&gt;.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P class="lia-align-justify"&gt;They might be useful.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 18:50:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-Internal-Voltage-Ref-to-ADC/m-p/1584146#M51300</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-01-17T18:50:44Z</dc:date>
    </item>
  </channel>
</rss>