<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PowerQuad on LPC55S66 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/PowerQuad-on-LPC55S66/m-p/1582962#M51280</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I see that the LPC55S66 has just 144K SRAM and does not have RAM4 memory.&lt;/P&gt;
&lt;P&gt;I will ask the AE team if the PowerQuad can work without RAM4 module. Pls be patient.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Mon, 16 Jan 2023 07:14:19 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-01-16T07:14:19Z</dc:date>
    <item>
      <title>PowerQuad on LPC55S66</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PowerQuad-on-LPC55S66/m-p/1582752#M51275</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;According to UM11126:&lt;/P&gt;&lt;P&gt;In the LPC55S6x, the PowerQuad uses SRAM Bank 4 (16kB at 0x2004 0000 to 3FFF&lt;BR /&gt;or 0x3004 0000 to 3FFF depending on the Secured or Non Secured Configuration) for&lt;BR /&gt;scratch pad.&lt;/P&gt;&lt;P&gt;However there is no SRAM4 on 144KB devices:&lt;/P&gt;&lt;TABLE border="1" width="79.01229193162136%"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="10%"&gt;RAM Total&lt;/TD&gt;&lt;TD width="10%"&gt;RAM-X (KB)&lt;/TD&gt;&lt;TD width="10%"&gt;RAM0 (KB)&lt;/TD&gt;&lt;TD width="10%"&gt;RAM1 (KB)&lt;/TD&gt;&lt;TD width="10%"&gt;RAM2 (KB)&lt;/TD&gt;&lt;TD width="10%"&gt;RAM3 (KB)&lt;/TD&gt;&lt;TD width="10%"&gt;RAM4 (KB)&lt;/TD&gt;&lt;TD width="10%"&gt;USB-RAM (KB)&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="10%"&gt;144 KB devices&lt;/TD&gt;&lt;TD width="10%"&gt;32&lt;/TD&gt;&lt;TD width="10%"&gt;64&lt;/TD&gt;&lt;TD width="10%"&gt;32&lt;/TD&gt;&lt;TD width="10%"&gt;-&lt;/TD&gt;&lt;TD width="10%"&gt;-&lt;/TD&gt;&lt;TD width="10%"&gt;-&lt;/TD&gt;&lt;TD width="10%"&gt;16&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So does&amp;nbsp;PowerQuad works on this part ?&lt;/P&gt;</description>
      <pubDate>Sat, 14 Jan 2023 17:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PowerQuad-on-LPC55S66/m-p/1582752#M51275</guid>
      <dc:creator>zixunli</dc:creator>
      <dc:date>2023-01-14T17:56:01Z</dc:date>
    </item>
    <item>
      <title>Re: PowerQuad on LPC55S66</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PowerQuad-on-LPC55S66/m-p/1582962#M51280</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I see that the LPC55S66 has just 144K SRAM and does not have RAM4 memory.&lt;/P&gt;
&lt;P&gt;I will ask the AE team if the PowerQuad can work without RAM4 module. Pls be patient.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 07:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PowerQuad-on-LPC55S66/m-p/1582962#M51280</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-01-16T07:14:19Z</dc:date>
    </item>
    <item>
      <title>Re: PowerQuad on LPC55S66</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PowerQuad-on-LPC55S66/m-p/1590236#M51453</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This is the AE team reply:&lt;/P&gt;
&lt;P&gt;"PQ can work with LPC55S66. The use of RAM4 is optional, if using RAM4, QR can reach best performance, with PQ can also use other RAM area.&lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;
&lt;P&gt;It means that the PowerQuad of LPC55S66 can work without RAM4 module.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 03:27:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PowerQuad-on-LPC55S66/m-p/1590236#M51453</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-01-31T03:27:15Z</dc:date>
    </item>
    <item>
      <title>Re: PowerQuad on LPC55S66</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PowerQuad-on-LPC55S66/m-p/1590666#M51462</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Could you give me more detail:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;What's the performance difference if RAM4 is not used ?&lt;/LI&gt;&lt;LI&gt;How to use other RAM area ? I haven't found any information in reference manual and in kSDK.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 15:12:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PowerQuad-on-LPC55S66/m-p/1590666#M51462</guid>
      <dc:creator>zixunli</dc:creator>
      <dc:date>2023-01-31T15:12:55Z</dc:date>
    </item>
  </channel>
</rss>