<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックMCU-Link pro powering a LPC54S018-EVK</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-Link-pro-powering-a-LPC54S018-EVK/m-p/1581187#M51254</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have been using a LPC54S018-EVK board with a Dual CAN-FD Shield (OM13099). I have used my written software as well as provided SDK example "mcan_interrupt_transfer" to send and receive data through the CAN shield while using the debug probe that comes with the LPC54S018-EVK board; However, I was trying to use a MCU-Link pro instead and I ran into an issue. While powering the LPC54S018 board from MCU-Link pro, the CAN shield seems to not get enough power to function properly.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;What I have done:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Set JP6 on MCU-Link pro (to power target board)&lt;/LI&gt;&lt;LI&gt;connect the 10-way SWD ribbon cable from J7 on MCU-Link pro to SWD on LPC54S018&lt;/LI&gt;&lt;LI&gt;Connect VCOM IN&amp;nbsp; of MCU-Link pro to Tx on LPC54S018&lt;/LI&gt;&lt;LI&gt;Connect VCOM OUT of MCU-Link pro to Rx on LPC54S018&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;What works:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I can debug code&lt;/LI&gt;&lt;LI&gt;I can flash software to the LPC54S018-EVK board&lt;/LI&gt;&lt;LI&gt;I have access to COM port input and output&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;What does not work:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;CAN shield does not send/received data (also the LED on the CAN shield seems not as bright as usual)&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found out that powering the board separately using another USB cable connected to the "Power only" USB, solves the issue; However, I would like to power the board with MCU-Link pro if possible. I was wondering how I can do that.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Mohammad&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 11 Jan 2023 22:14:57 GMT</pubDate>
    <dc:creator>mh_n</dc:creator>
    <dc:date>2023-01-11T22:14:57Z</dc:date>
    <item>
      <title>MCU-Link pro powering a LPC54S018-EVK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-Link-pro-powering-a-LPC54S018-EVK/m-p/1581187#M51254</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have been using a LPC54S018-EVK board with a Dual CAN-FD Shield (OM13099). I have used my written software as well as provided SDK example "mcan_interrupt_transfer" to send and receive data through the CAN shield while using the debug probe that comes with the LPC54S018-EVK board; However, I was trying to use a MCU-Link pro instead and I ran into an issue. While powering the LPC54S018 board from MCU-Link pro, the CAN shield seems to not get enough power to function properly.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;What I have done:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Set JP6 on MCU-Link pro (to power target board)&lt;/LI&gt;&lt;LI&gt;connect the 10-way SWD ribbon cable from J7 on MCU-Link pro to SWD on LPC54S018&lt;/LI&gt;&lt;LI&gt;Connect VCOM IN&amp;nbsp; of MCU-Link pro to Tx on LPC54S018&lt;/LI&gt;&lt;LI&gt;Connect VCOM OUT of MCU-Link pro to Rx on LPC54S018&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;What works:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I can debug code&lt;/LI&gt;&lt;LI&gt;I can flash software to the LPC54S018-EVK board&lt;/LI&gt;&lt;LI&gt;I have access to COM port input and output&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;What does not work:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;CAN shield does not send/received data (also the LED on the CAN shield seems not as bright as usual)&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found out that powering the board separately using another USB cable connected to the "Power only" USB, solves the issue; However, I would like to power the board with MCU-Link pro if possible. I was wondering how I can do that.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Mohammad&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jan 2023 22:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-Link-pro-powering-a-LPC54S018-EVK/m-p/1581187#M51254</guid>
      <dc:creator>mh_n</dc:creator>
      <dc:date>2023-01-11T22:14:57Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-Link pro powering a LPC54S018-EVK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-Link-pro-powering-a-LPC54S018-EVK/m-p/1581344#M51255</link>
      <description>&lt;P&gt;Hi, Mohammad,&lt;/P&gt;
&lt;P&gt;You want to connect only the MCU-LINK Pro with USB, and power all LPC54S018-EVK and Dual CAN-FD Shield from MCU-LINK Pro, it is NOT possible from design.&lt;/P&gt;
&lt;P&gt;From the following circuit, the Pin1 of P1 connector can get 3.3V power from the MCU-LINK Pro, but it can not power the&amp;nbsp;VDD_TARGET node even if you close the pin2&amp;amp;3 of JP2. In other words, the LPC54S018-EVK can not get power from MCU-LINK Pro.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1673494380899.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/206990i56F7E28333582D0A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1673494380899.png" alt="xiangjun_rong_0-1673494380899.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1673494380899.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest you power the LPC54S018-EVK and Dual CAN-FD Shield with the J1 power only USB connector, and connect the MCU-LINK Pro with another USB connector as you have done.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jan 2023 03:38:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCU-Link-pro-powering-a-LPC54S018-EVK/m-p/1581344#M51255</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-01-12T03:38:46Z</dc:date>
    </item>
  </channel>
</rss>