<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Dual-single-ended mode for LPC55s69's ADC in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-single-ended-mode-for-LPC55s69-s-ADC/m-p/1578700#M51214</link>
    <description>&lt;P&gt;I am attempting to use the ADC in dual single ended mode (user manual section 39.6.16, ADC command low buffer registers, CTYPE == 0x03) on the LPC55s69 but so far I have not been successful. Other chips in the family (LPC553x) appear to have a very similar ADC and have a few added bits/fields in the same register that seem to pertain to this mode. But the corresponding bits/fields in the LPC55s69's user manual are reserved.&lt;/P&gt;&lt;P&gt;Has anyone else had any success using the ADC in dual single ended mode? Is this feature not supported in the LPC55s69?&lt;/P&gt;</description>
    <pubDate>Fri, 06 Jan 2023 19:28:39 GMT</pubDate>
    <dc:creator>plong44</dc:creator>
    <dc:date>2023-01-06T19:28:39Z</dc:date>
    <item>
      <title>Dual-single-ended mode for LPC55s69's ADC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-single-ended-mode-for-LPC55s69-s-ADC/m-p/1578700#M51214</link>
      <description>&lt;P&gt;I am attempting to use the ADC in dual single ended mode (user manual section 39.6.16, ADC command low buffer registers, CTYPE == 0x03) on the LPC55s69 but so far I have not been successful. Other chips in the family (LPC553x) appear to have a very similar ADC and have a few added bits/fields in the same register that seem to pertain to this mode. But the corresponding bits/fields in the LPC55s69's user manual are reserved.&lt;/P&gt;&lt;P&gt;Has anyone else had any success using the ADC in dual single ended mode? Is this feature not supported in the LPC55s69?&lt;/P&gt;</description>
      <pubDate>Fri, 06 Jan 2023 19:28:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-single-ended-mode-for-LPC55s69-s-ADC/m-p/1578700#M51214</guid>
      <dc:creator>plong44</dc:creator>
      <dc:date>2023-01-06T19:28:39Z</dc:date>
    </item>
    <item>
      <title>Re: Dual-single-ended mode for LPC55s69's ADC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-single-ended-mode-for-LPC55s69-s-ADC/m-p/1579815#M51227</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178795"&gt;@plong44&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can try to use MCUXpresso config tool for peripheral to config:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1673334480070.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/206637i5554D2877B1C7BE9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1673334480070.png" alt="Alice_Yang_0-1673334480070.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_0-1673334480070.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Jan 2023 07:08:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-single-ended-mode-for-LPC55s69-s-ADC/m-p/1579815#M51227</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-01-10T07:08:10Z</dc:date>
    </item>
  </channel>
</rss>