<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S28-EVK USB MSC HS Demo in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-EVK-USB-MSC-HS-Demo/m-p/1576717#M51172</link>
    <description>&lt;P&gt;For an additional datapoint, I added some logging to the USB_DeviceCallback(), and the high speed enumeration gets stuck on the event kUSB_DeviceEventBusReset.&lt;/P&gt;</description>
    <pubDate>Tue, 03 Jan 2023 21:12:12 GMT</pubDate>
    <dc:creator>fingew</dc:creator>
    <dc:date>2023-01-03T21:12:12Z</dc:date>
    <item>
      <title>LPC55S28-EVK USB MSC HS Demo</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-EVK-USB-MSC-HS-Demo/m-p/1575648#M51134</link>
      <description>&lt;P&gt;I am attempting to use the example in the SDK, "usb_device_msc_disk", with my LOPC55S28-EVK board.&amp;nbsp; The example works fine in full-speed.&lt;/P&gt;&lt;P&gt;However, I would like it to work in high-speed.&amp;nbsp; If I edit the file "usb_device_config.h" and change&amp;nbsp;USB_DEVICE_CONFIG_LPCIP3511FS&amp;nbsp; to 0 and&amp;nbsp;USB_DEVICE_CONFIG_LPCIP3511HS to 1, the PC attempts to connect to the board via the HS connection (P9), but fails and gives and error (device not recognized).&lt;/P&gt;&lt;P&gt;Is there another setting I need to change for this to work?&lt;/P&gt;&lt;P&gt;Alternatively, is there another example in the SDK that works with HS interface?&amp;nbsp; They all seem to be configured for FS by default.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Dec 2022 20:06:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-EVK-USB-MSC-HS-Demo/m-p/1575648#M51134</guid>
      <dc:creator>fingew</dc:creator>
      <dc:date>2022-12-29T20:06:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28-EVK USB MSC HS Demo</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-EVK-USB-MSC-HS-Demo/m-p/1576337#M51165</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192282"&gt;@fingew&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can have a look at:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC-ALL-Summary-of-Switching-USB-demo-from-USB0-to-USB1/ta-p/1428522" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC-ALL-Summary-of-Switching-USB-demo-from-USB0-to-USB1/ta-p/1428522&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Especially:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1672726085068.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205918i79D3763BC208AEE8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1672726085068.png" alt="Alice_Yang_0-1672726085068.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_0-1672726085068.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jan 2023 06:08:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-EVK-USB-MSC-HS-Demo/m-p/1576337#M51165</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-01-03T06:08:28Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28-EVK USB MSC HS Demo</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-EVK-USB-MSC-HS-Demo/m-p/1576630#M51168</link>
      <description>&lt;P&gt;Alice,&lt;/P&gt;&lt;P&gt;Thank you for your response.&amp;nbsp; The only text the UM has regarding USB on this EVM is this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fingew_0-1672759008195.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205968iA02CEA7F9BC827DD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="fingew_0-1672759008195.png" alt="fingew_0-1672759008195.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;fingew_0-1672759008195.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Since I'm not using Host mode, I have long since removed J6.&amp;nbsp; I also removed R84 (the pulldown in the VBUS detection circuit) which was populated on my board:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fingew_1-1672759270126.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205969iF84347ACAFD8025D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="fingew_1-1672759270126.png" alt="fingew_1-1672759270126.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;fingew_1-1672759270126.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any other hints?&amp;nbsp; I've tried two demo projects thus far and both have yielded the same failure.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;&lt;SPAN&gt;Bill&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jan 2023 15:22:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-EVK-USB-MSC-HS-Demo/m-p/1576630#M51168</guid>
      <dc:creator>fingew</dc:creator>
      <dc:date>2023-01-03T15:22:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28-EVK USB MSC HS Demo</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-EVK-USB-MSC-HS-Demo/m-p/1576717#M51172</link>
      <description>&lt;P&gt;For an additional datapoint, I added some logging to the USB_DeviceCallback(), and the high speed enumeration gets stuck on the event kUSB_DeviceEventBusReset.&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jan 2023 21:12:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-EVK-USB-MSC-HS-Demo/m-p/1576717#M51172</guid>
      <dc:creator>fingew</dc:creator>
      <dc:date>2023-01-03T21:12:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28-EVK USB MSC HS Demo</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-EVK-USB-MSC-HS-Demo/m-p/1578044#M51195</link>
      <description>&lt;P&gt;I figured out the problem.&amp;nbsp; I didn't have __usb_use_usbram__=1 in my linker settings, and so the application silently failed.&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 14:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-EVK-USB-MSC-HS-Demo/m-p/1578044#M51195</guid>
      <dc:creator>fingew</dc:creator>
      <dc:date>2023-01-05T14:29:48Z</dc:date>
    </item>
  </channel>
</rss>