<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックhow to enter ISP mode via user application--LPC Board</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1574950#M51115</link>
    <description>&lt;P&gt;Hi all,&lt;BR /&gt;i am trying to find API for entering in UART ISP mode in LPC board.&lt;BR /&gt;There is a firmware which is up and running on the board, from that firmware, i need to call the API to enter into ISP mode.&lt;BR /&gt;can anyone guide me on this, if it is possible from user application?&lt;BR /&gt;is there any application note or example is available for the same?&lt;/P&gt;&lt;P&gt;can anyone guide for the application note for communicating in ISP mode using blhost?&lt;/P&gt;&lt;P&gt;Thanks in Advance.&lt;/P&gt;</description>
    <pubDate>Thu, 05 Jan 2023 14:04:08 GMT</pubDate>
    <dc:creator>anshulkhare</dc:creator>
    <dc:date>2023-01-05T14:04:08Z</dc:date>
    <item>
      <title>how to enter ISP mode via user application--LPC Board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1574950#M51115</link>
      <description>&lt;P&gt;Hi all,&lt;BR /&gt;i am trying to find API for entering in UART ISP mode in LPC board.&lt;BR /&gt;There is a firmware which is up and running on the board, from that firmware, i need to call the API to enter into ISP mode.&lt;BR /&gt;can anyone guide me on this, if it is possible from user application?&lt;BR /&gt;is there any application note or example is available for the same?&lt;/P&gt;&lt;P&gt;can anyone guide for the application note for communicating in ISP mode using blhost?&lt;/P&gt;&lt;P&gt;Thanks in Advance.&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 14:04:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1574950#M51115</guid>
      <dc:creator>anshulkhare</dc:creator>
      <dc:date>2023-01-05T14:04:08Z</dc:date>
    </item>
    <item>
      <title>Re: how to enter ISP mode via user application--LPC55S06</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1575007#M51117</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I review your information and I recommend review the RunBootloader API chapter&amp;nbsp;9.3.4 in User Manual.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;The ROM bootloader provides an API for the user application to enter the ISP mode&lt;/EM&gt;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&lt;EM&gt;based on the designated ISP interface mode.&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;And suggest review the documentation for the blhost. &lt;A href="https://www.nxp.com/docs/en/user-guide/MCUBLHOSTUG.pdf" target="_blank"&gt;MCUBLHOSTUG.pdf (nxp.com)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This thread maybe could help you.&amp;nbsp;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/Configure-LPC55-to-enter-re-invoke-ROM-Bootloader-from/m-p/966990" target="_blank"&gt;Solved: Configure LPC55 to enter/re-invoke ROM Bootloader ... - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;If you have more questions, please let me know.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 27 Dec 2022 22:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1575007#M51117</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-12-27T22:09:12Z</dc:date>
    </item>
    <item>
      <title>Re: how to enter ISP mode via user application--LPC Board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1583083#M51281</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196430"&gt;@Pavel_Hernandez&lt;/a&gt;&amp;nbsp;Thanks for your reply.&lt;/P&gt;&lt;P&gt;in ISP mode can we upgrade signed image on the chip where security is enabled, using blhost?&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 09:49:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1583083#M51281</guid>
      <dc:creator>anshulkhare</dc:creator>
      <dc:date>2023-01-16T09:49:16Z</dc:date>
    </item>
    <item>
      <title>Re: how to enter ISP mode via user application--LPC Board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1583491#M51286</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;If you mean "security is enabled" is the "secure boot" turned on, so you can't&amp;nbsp;program a new image anymore.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 00:02:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1583491#M51286</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-01-17T00:02:35Z</dc:date>
    </item>
    <item>
      <title>Re: how to enter ISP mode via user application--LPC Board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1583681#M51289</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196430"&gt;@Pavel_Hernandez&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;does it mean if secure boot is enabled ,in that case user application can not be upgrade using ISP or IAP?&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 06:00:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1583681#M51289</guid>
      <dc:creator>anshulkhare</dc:creator>
      <dc:date>2023-01-17T06:00:37Z</dc:date>
    </item>
    <item>
      <title>Re: how to enter ISP mode via user application--LPC Board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1584223#M51303</link>
      <description>&lt;P&gt;All ISP, JTAG. IAP can be used to program after enabling a secure boot. but you must use it program&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;signed image,&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;otherwise, it can't pass the secure boot check.&lt;/P&gt;
&lt;P&gt;It's not possible to program the flash with IDE debug because it's not a signed image when debugging code.&lt;/P&gt;
&lt;P&gt;AN12283&amp;nbsp;LPC55Sxx Secure Boot&lt;BR /&gt;AN13037 LPC55Sxx Debug Authentication&lt;/P&gt;
&lt;P&gt;Maybe that app note could help you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 00:03:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-enter-ISP-mode-via-user-application-LPC-Board/m-p/1584223#M51303</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-01-18T00:03:37Z</dc:date>
    </item>
  </channel>
</rss>