<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックI2C Detection Fail</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/I2C-Detection-Fail/m-p/1574235#M51095</link>
    <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I have a problem with the OM40001 sample "lpcxpresso804_lpc_i2c_interrupt_b2b_transfer_slave". I have removed the bridges for the LM75 and agreed on a slave on SCL PIO0_14 and SDA PIO0_7. I can't find the device on my agreed address with an I2C detect with an I2C master. I have connected SCL with SCL and SDA with SDA.&lt;BR /&gt;Does anyone have a solution? Thanks a lot.&lt;/P&gt;</description>
    <pubDate>Fri, 23 Dec 2022 16:16:36 GMT</pubDate>
    <dc:creator>coder_72</dc:creator>
    <dc:date>2022-12-23T16:16:36Z</dc:date>
    <item>
      <title>I2C Detection Fail</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/I2C-Detection-Fail/m-p/1574235#M51095</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I have a problem with the OM40001 sample "lpcxpresso804_lpc_i2c_interrupt_b2b_transfer_slave". I have removed the bridges for the LM75 and agreed on a slave on SCL PIO0_14 and SDA PIO0_7. I can't find the device on my agreed address with an I2C detect with an I2C master. I have connected SCL with SCL and SDA with SDA.&lt;BR /&gt;Does anyone have a solution? Thanks a lot.&lt;/P&gt;</description>
      <pubDate>Fri, 23 Dec 2022 16:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/I2C-Detection-Fail/m-p/1574235#M51095</guid>
      <dc:creator>coder_72</dc:creator>
      <dc:date>2022-12-23T16:16:36Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Detection Fail</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/I2C-Detection-Fail/m-p/1574375#M51098</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I have downloaded the data sheet of LM75, which is a temperature sensor with I2C interface, but the LPC75 can only be a I2C slave in stead of master, if you use the I2C module of LPC804 with SCL PIO0_14 and SDA PIO0_7, the I2C module of LPC804 is master.&lt;/P&gt;
&lt;P&gt;For the device address of LM75, it has A2/A1/A0 pins, this is address format.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1672022324982.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205400i3C8760B4D848F6D5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1672022324982.png" alt="xiangjun_rong_0-1672022324982.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1672022324982.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Assume that the A2/A1/A0 pin logic is 000 via pull up/down resistors, the I2C device address of LM75 is 0x48. Assume that the A2/A1/A0 pin logic is 011, the I2C device address of LM75 is 0x4B.&lt;/P&gt;
&lt;P&gt;Because the I2C of LPC804 is master, so you have to use the&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_2-1672022619602.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205403i219E5B25ADA2D523/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_2-1672022619602.png" alt="xiangjun_rong_2-1672022619602.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_2-1672022619602.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 26 Dec 2022 02:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/I2C-Detection-Fail/m-p/1574375#M51098</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-12-26T02:47:30Z</dc:date>
    </item>
  </channel>
</rss>