<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC802, SWD disabling in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-SWD-disabling/m-p/1572427#M51058</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I disable SWD in LPC802 because I need to use PIO0_2 and PIO0_3 as general purpose outputs. Is it&amp;nbsp; mandatory to disable SWD to use these ports as general output ?&lt;/P&gt;&lt;P&gt;On the other hand, once I disable SWD ("__CRP const unsigned int CRP_WORD = CRP_CRP1;") I can no longer access LPC802. I put ISP pin low but LPC802 is not detected via SWD. Is that correct? How do I flash LPC802 via SWD again?&lt;/P&gt;&lt;P&gt;Thanks is advance,&lt;/P&gt;&lt;P&gt;Asier.&lt;/P&gt;</description>
    <pubDate>Tue, 20 Dec 2022 09:22:48 GMT</pubDate>
    <dc:creator>asier</dc:creator>
    <dc:date>2022-12-20T09:22:48Z</dc:date>
    <item>
      <title>LPC802, SWD disabling</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-SWD-disabling/m-p/1572427#M51058</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I disable SWD in LPC802 because I need to use PIO0_2 and PIO0_3 as general purpose outputs. Is it&amp;nbsp; mandatory to disable SWD to use these ports as general output ?&lt;/P&gt;&lt;P&gt;On the other hand, once I disable SWD ("__CRP const unsigned int CRP_WORD = CRP_CRP1;") I can no longer access LPC802. I put ISP pin low but LPC802 is not detected via SWD. Is that correct? How do I flash LPC802 via SWD again?&lt;/P&gt;&lt;P&gt;Thanks is advance,&lt;/P&gt;&lt;P&gt;Asier.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 09:22:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-SWD-disabling/m-p/1572427#M51058</guid>
      <dc:creator>asier</dc:creator>
      <dc:date>2022-12-20T09:22:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC802, SWD disabling</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-SWD-disabling/m-p/1573075#M51062</link>
      <description>&lt;P&gt;Hi&amp;nbsp;asier&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You want to set PIO_2 PIO_3 as GPIO, no need to set CRP1 to disable SWD. Just set the pin in SWM module. Set SWDIO to connect P0_2 and P0_3.&lt;/P&gt;
&lt;P&gt;If you already enabled CRP1. Doing mass erase in ISP mode can recover it.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1671615620926.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205130iF40DFF2275E6F29D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1671615620926.png" alt="ZhangJennie_0-1671615620926.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ZhangJennie_0-1671615620926.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Fri, 23 Dec 2022 10:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-SWD-disabling/m-p/1573075#M51062</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-12-23T10:15:08Z</dc:date>
    </item>
  </channel>
</rss>