<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC54S0xx Looking for base address of BOOT ROM RSA API</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S0xx-Looking-for-base-address-of-BOOT-ROM-RSA-API/m-p/1562995#M50916</link>
    <description>Hi Alice,&lt;BR /&gt;&lt;BR /&gt;No the address 0x0300 023C also doesn't work.&lt;BR /&gt;&lt;BR /&gt;Regards,</description>
    <pubDate>Thu, 01 Dec 2022 20:43:21 GMT</pubDate>
    <dc:creator>gtkp</dc:creator>
    <dc:date>2022-12-01T20:43:21Z</dc:date>
    <item>
      <title>LPC54S0xx Looking for base address of BOOT ROM RSA API</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S0xx-Looking-for-base-address-of-BOOT-ROM-RSA-API/m-p/1560173#M50848</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm reading UM11060, Chapter 45.7 RSA API.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;The boot ROM provides APIs to perform RSA2048 signature checking routines in&lt;BR /&gt;application code.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;It goes on to show a table of functions with their offset.&amp;nbsp; Offset to where?&amp;nbsp; All I can find in the document is that Boot Rom is between 0x0300 0000 and 0x0300 FFFF.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Applying the offsets to the start of Boot ROM yields a Hard fault for undefined instruction so that is clearly not the correct base address.&amp;nbsp; The document does mention that the ROM driver table is at 0x300 0200 and offsets are given for the USB, OTP, AES, RNG but not for the RSA API.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where is a complete document of the ROM driver table for #LPC54S0xx ?&lt;/P&gt;</description>
      <pubDate>Sat, 26 Nov 2022 23:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S0xx-Looking-for-base-address-of-BOOT-ROM-RSA-API/m-p/1560173#M50848</guid>
      <dc:creator>gtkp</dc:creator>
      <dc:date>2022-11-26T23:32:20Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54S0xx Looking for base address of BOOT ROM RSA API</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S0xx-Looking-for-base-address-of-BOOT-ROM-RSA-API/m-p/1562545#M50897</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203011"&gt;@gtkp&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Try to&amp;nbsp; address 0x0300 023C ?&lt;/P&gt;
&lt;P&gt;If still can not work, please tell me.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 05:35:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S0xx-Looking-for-base-address-of-BOOT-ROM-RSA-API/m-p/1562545#M50897</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-12-01T05:35:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54S0xx Looking for base address of BOOT ROM RSA API</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S0xx-Looking-for-base-address-of-BOOT-ROM-RSA-API/m-p/1562995#M50916</link>
      <description>Hi Alice,&lt;BR /&gt;&lt;BR /&gt;No the address 0x0300 023C also doesn't work.&lt;BR /&gt;&lt;BR /&gt;Regards,</description>
      <pubDate>Thu, 01 Dec 2022 20:43:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S0xx-Looking-for-base-address-of-BOOT-ROM-RSA-API/m-p/1562995#M50916</guid>
      <dc:creator>gtkp</dc:creator>
      <dc:date>2022-12-01T20:43:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54S0xx Looking for base address of BOOT ROM RSA API</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S0xx-Looking-for-base-address-of-BOOT-ROM-RSA-API/m-p/1569527#M51018</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203011"&gt;@gtkp&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I have escalate this issue to DOC and SDK team, they still working on it.&lt;/P&gt;
&lt;P&gt;And the latest reply is there is no RSA API in BOOT ROM code.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 09:00:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S0xx-Looking-for-base-address-of-BOOT-ROM-RSA-API/m-p/1569527#M51018</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-12-14T09:00:31Z</dc:date>
    </item>
  </channel>
</rss>