<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55 Flash in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-Flash/m-p/1560738#M50851</link>
    <description>&lt;P&gt;Call FLASH_Program write 512 bytes, Then call FLASH_VerifyProgram for validation，FLASH_Program returns normal, but FLASH_VerifyProgram returns error code 116， &amp;nbsp;Next, write according to the flash address order, and the error code returned by the FLASH_Program is 102，&lt;/P&gt;&lt;P&gt;&amp;nbsp;After the above problem, it is found that the part of the corresponding flash address that has no operation, such as bootloader, has also been abnormal.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;Help confirm that when this error code appears, what operations are done inside the chip?&lt;/P&gt;</description>
    <pubDate>Mon, 28 Nov 2022 15:03:08 GMT</pubDate>
    <dc:creator>Zhang_123</dc:creator>
    <dc:date>2022-11-28T15:03:08Z</dc:date>
    <item>
      <title>LPC55 Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-Flash/m-p/1560738#M50851</link>
      <description>&lt;P&gt;Call FLASH_Program write 512 bytes, Then call FLASH_VerifyProgram for validation，FLASH_Program returns normal, but FLASH_VerifyProgram returns error code 116， &amp;nbsp;Next, write according to the flash address order, and the error code returned by the FLASH_Program is 102，&lt;/P&gt;&lt;P&gt;&amp;nbsp;After the above problem, it is found that the part of the corresponding flash address that has no operation, such as bootloader, has also been abnormal.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;Help confirm that when this error code appears, what operations are done inside the chip?&lt;/P&gt;</description>
      <pubDate>Mon, 28 Nov 2022 15:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-Flash/m-p/1560738#M50851</guid>
      <dc:creator>Zhang_123</dc:creator>
      <dc:date>2022-11-28T15:03:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55 Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-Flash/m-p/1562499#M50894</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195817"&gt;@Zhang_123&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please tell the whole part number of your chip, for example L&lt;SPAN&gt;PC55S69JBD100.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 02:58:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-Flash/m-p/1562499#M50894</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-12-01T02:58:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55 Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-Flash/m-p/1562557#M50899</link>
      <description>&lt;P&gt;The full part number is &lt;SPAN&gt;LPC55S26JBD64Y&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 05:56:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-Flash/m-p/1562557#M50899</guid>
      <dc:creator>Zhang_123</dc:creator>
      <dc:date>2022-12-01T05:56:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55 Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-Flash/m-p/1562731#M50907</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195817"&gt;@Zhang_123&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For this part, the Flash size customer can use is 256K.&lt;/P&gt;
&lt;P&gt;About Flashapi using, you can refer to SDK demo "flashiap1":&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1669887732836.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/202423i39ECB799DBEBD13D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1669887732836.png" alt="Alice_Yang_0-1669887732836.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 09:42:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-Flash/m-p/1562731#M50907</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-12-01T09:42:48Z</dc:date>
    </item>
  </channel>
</rss>