<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1114/444FBD48 IAP Code Size Issue</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114-444FBD48-IAP-Code-Size-Issue/m-p/1558226#M50796</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suggest you generate a memory map file based on your application code with Keil and check if the code/constant data are saved in flash correctly, if there is issue, check if the linker file has issue.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Wed, 23 Nov 2022 06:17:43 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2022-11-23T06:17:43Z</dc:date>
    <item>
      <title>LPC1114/444FBD48 IAP Code Size Issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114-444FBD48-IAP-Code-Size-Issue/m-p/1557776#M50791</link>
      <description>&lt;P&gt;I am using NXP LPC1114/333 (56K flash) with keil 5.&lt;BR /&gt;Bootloader starts from 0 and App starts at 0x1000&lt;BR /&gt;App works fine when BIN size is 24,384 Bytes or smaller:&lt;BR /&gt;Program Size: Code=22604 RO-data=1452 RW-data=1020 ZI-data=1228&lt;/P&gt;&lt;P&gt;But not larger.&lt;BR /&gt;When I set App runs from 0, the flash size limit issue is gone, so codes were fine.&lt;/P&gt;&lt;P&gt;Where should I start to get rid of this?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;ZQ&lt;/P&gt;</description>
      <pubDate>Tue, 22 Nov 2022 11:20:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114-444FBD48-IAP-Code-Size-Issue/m-p/1557776#M50791</guid>
      <dc:creator>john_zhou1</dc:creator>
      <dc:date>2022-11-22T11:20:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1114/444FBD48 IAP Code Size Issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114-444FBD48-IAP-Code-Size-Issue/m-p/1558226#M50796</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suggest you generate a memory map file based on your application code with Keil and check if the code/constant data are saved in flash correctly, if there is issue, check if the linker file has issue.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 23 Nov 2022 06:17:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114-444FBD48-IAP-Code-Size-Issue/m-p/1558226#M50796</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-11-23T06:17:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1114/444FBD48 IAP Code Size Issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114-444FBD48-IAP-Code-Size-Issue/m-p/1559142#M50820</link>
      <description>&lt;P&gt;Hello dear xiangjun_rong:&lt;/P&gt;&lt;P&gt;Thanks for the fast reply.&lt;/P&gt;&lt;P&gt;I have generated Maps for both working and not working BINs and did not have any clues.&lt;/P&gt;&lt;P&gt;I am located in Beijing, China. May I request an offline support or phone call?&amp;nbsp;Because this is urgent, even paid tech support are acceptable.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 24 Nov 2022 06:26:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114-444FBD48-IAP-Code-Size-Issue/m-p/1559142#M50820</guid>
      <dc:creator>john_zhou1</dc:creator>
      <dc:date>2022-11-24T06:26:36Z</dc:date>
    </item>
  </channel>
</rss>