<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC80X | looking for Ture random function in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1557785#M50793</link>
    <description>&lt;P&gt;Could you possibly use the Unique_ID which each IC has?&amp;nbsp;&lt;/P&gt;&lt;P&gt;u32 NXP_Unique_ID;&lt;/P&gt;&lt;P&gt;NXP_Unique_ID = Chip_IAP_ReadUID(); //32 bit UID&lt;/P&gt;&lt;P&gt;Byte_ID_3 = NXP_Unique_ID &amp;gt;&amp;gt; 24; //3&lt;BR /&gt;Byte_ID_2 = NXP_Unique_ID &amp;gt;&amp;gt; 16; //2&lt;BR /&gt;Byte_ID_1 = NXP_Unique_ID &amp;gt;&amp;gt; 8; //1&lt;BR /&gt;Byte_ID_0 = NXP_Unique_ID; //0&lt;/P&gt;&lt;P&gt;Regards Sanders7284&lt;/P&gt;</description>
    <pubDate>Tue, 22 Nov 2022 11:35:17 GMT</pubDate>
    <dc:creator>sanders7284</dc:creator>
    <dc:date>2022-11-22T11:35:17Z</dc:date>
    <item>
      <title>LPC80X | looking for Ture random function</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1528797#M50282</link>
      <description>&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;I am working on LPC802 and I was looking for secure random function (should provide unique random number each MCU).&lt;/P&gt;&lt;P&gt;I know on the LPC was an RNG driver which provide with true random function, but I did not found such a driver into the lpc802 SDK.&lt;/P&gt;&lt;P&gt;Can you please advise back how do I perform such true random function (with unique seed) with lpc802?&lt;/P&gt;&lt;P&gt;Waiting for your kind feedback, thanks in advance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Shai Berman&lt;/P&gt;</description>
      <pubDate>Tue, 27 Sep 2022 11:59:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1528797#M50282</guid>
      <dc:creator>shai_b</dc:creator>
      <dc:date>2022-09-27T11:59:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC80X | looking for Ture random function</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1529199#M50292</link>
      <description>&lt;P&gt;Hi, Shai,&lt;/P&gt;
&lt;P&gt;Regarding the Random Number Generation, there are two methods to generate the RND number, one is to use RNG hardware module, another is to use pure firmware. But the LPC8xx neither have the RNG module from hardware perspective,&amp;nbsp; nor have the source code or library in SDK.&lt;/P&gt;
&lt;P&gt;I have checked the mbedtls library which is only for Cortex-M4, it has implemented the rand() function.&lt;/P&gt;
&lt;P&gt;I attach the example of mbedtls based on &lt;STRONG&gt;LPC54628&lt;/STRONG&gt; which uses Cortex-M4 core.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1664340753636.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/195102iBB11C71F99175DDD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1664340753636.png" alt="xiangjun_rong_0-1664340753636.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1664340753636.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 04:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1529199#M50292</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-09-28T04:57:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC80X | looking for Ture random function</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1540384#M50452</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your comments but using rand(); function will not produce a real true random number.&lt;/P&gt;&lt;P&gt;It's a kind of hash technique that generates a new number (with wrapping) based on the given seed number but it will produce the same "random" number each time.&lt;/P&gt;&lt;P&gt;it's not good for my use case. thanks again for your input.&lt;/P&gt;&lt;P&gt;KR,&lt;/P&gt;&lt;P&gt;Shai&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 20:02:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1540384#M50452</guid>
      <dc:creator>shai_b</dc:creator>
      <dc:date>2022-10-19T20:02:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC80X | looking for Ture random function</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1540751#M50453</link>
      <description>&lt;P&gt;A really random value is difficult to achieve, especially on a MCU with relatively little resources.&lt;/P&gt;&lt;P&gt;One of my former companies used noisy input of an ADC for this purpose. This was a 8-bit architecture, though.&lt;/P&gt;&lt;P&gt;Here an article from another vendor as example, for a Cortex M :&amp;nbsp;&lt;A href="https://siliconlabs.force.com/community/s/article/generating-an-8-bit-random-number-using-adc?language=en_US" target="_blank"&gt;https://siliconlabs.force.com/community/s/article/generating-an-8-bit-random-number-using-adc?language=en_US&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 05:14:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1540751#M50453</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2022-10-20T05:14:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC80X | looking for Ture random function</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1557785#M50793</link>
      <description>&lt;P&gt;Could you possibly use the Unique_ID which each IC has?&amp;nbsp;&lt;/P&gt;&lt;P&gt;u32 NXP_Unique_ID;&lt;/P&gt;&lt;P&gt;NXP_Unique_ID = Chip_IAP_ReadUID(); //32 bit UID&lt;/P&gt;&lt;P&gt;Byte_ID_3 = NXP_Unique_ID &amp;gt;&amp;gt; 24; //3&lt;BR /&gt;Byte_ID_2 = NXP_Unique_ID &amp;gt;&amp;gt; 16; //2&lt;BR /&gt;Byte_ID_1 = NXP_Unique_ID &amp;gt;&amp;gt; 8; //1&lt;BR /&gt;Byte_ID_0 = NXP_Unique_ID; //0&lt;/P&gt;&lt;P&gt;Regards Sanders7284&lt;/P&gt;</description>
      <pubDate>Tue, 22 Nov 2022 11:35:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1557785#M50793</guid>
      <dc:creator>sanders7284</dc:creator>
      <dc:date>2022-11-22T11:35:17Z</dc:date>
    </item>
    <item>
      <title>Re: LPC80X | looking for Ture random function</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1559176#M50821</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/161010"&gt;@sanders7284&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;This sounds like a good option to get a kinda random number so I could seed my rand() function with different seed numbers for each MCU.&lt;/P&gt;&lt;P&gt;Once I will implement that I will let you know if it works.&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Shai&lt;/P&gt;</description>
      <pubDate>Thu, 24 Nov 2022 07:22:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC80X-looking-for-Ture-random-function/m-p/1559176#M50821</guid>
      <dc:creator>shai_b</dc:creator>
      <dc:date>2022-11-24T07:22:22Z</dc:date>
    </item>
  </channel>
</rss>