<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC552x/S2x/S6x</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC552x-S2x-S6x/m-p/1555668#M50742</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;They might be simple questions, but nevertheless, I would like to verify..&lt;/P&gt;&lt;P&gt;1. I see that the "security" version of the&amp;nbsp;LPC55&lt;STRONG&gt;S28&lt;/STRONG&gt;JBD100 is more available than the non-secured (LPC55&lt;STRONG&gt;28&lt;/STRONG&gt;JBD100 ).&lt;/P&gt;&lt;P&gt;If I use the Secured version IC - can I consider it as 100% drop-in-replacement for the non-secured version? I.e - same SW and same HW (of course, without using the secured features that exist only in S version). assuming of course, that I refer to same package (i.e LQFP100).&lt;/P&gt;&lt;P&gt;2. On top of the last question, can I also consider the&amp;nbsp;&lt;STRONG&gt;LPC55S69JBD100&lt;/STRONG&gt;&amp;nbsp;as a replacement for the&amp;nbsp;&lt;STRONG&gt;LPC55S28JBD100&lt;/STRONG&gt;&amp;nbsp;if I do not use the "extra features" that the S69 ofers (i.e - dual core dsp accelerator) ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. Can I say that those 3 components has actually same pin functionality assuming I use the basic (or common) funciality of the &lt;STRONG&gt;LPC5528JBD100&lt;/STRONG&gt;&amp;nbsp;? which is another way to say that the S28 and S69 are based on the 28 with additional features.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;LPC5528JBD100&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;LPC55S28JBD100&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;LPC55S69JBD100&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to understand if any pin definitions as GPIO/UART/SPI/etc will be different for each of the above.&lt;/P&gt;&lt;P&gt;4. For SW aspect - can I burn same code for S and non-S version if the security-features are not used? or it will require different compilation for each?&lt;/P&gt;&lt;P&gt;I'm referring to the the product family comparison where I see that the "security system" is considered as "optional", so I guess that the SW/HW can be developed with the secured version but is only optional to be actually used:&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc5500-arm-cortex-m33:LPC5500_SERIES" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc5500-arm-cortex-m33:LPC5500_SERIES&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 17 Nov 2022 08:55:14 GMT</pubDate>
    <dc:creator>Uzi</dc:creator>
    <dc:date>2022-11-17T08:55:14Z</dc:date>
    <item>
      <title>LPC552x/S2x/S6x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC552x-S2x-S6x/m-p/1555668#M50742</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;They might be simple questions, but nevertheless, I would like to verify..&lt;/P&gt;&lt;P&gt;1. I see that the "security" version of the&amp;nbsp;LPC55&lt;STRONG&gt;S28&lt;/STRONG&gt;JBD100 is more available than the non-secured (LPC55&lt;STRONG&gt;28&lt;/STRONG&gt;JBD100 ).&lt;/P&gt;&lt;P&gt;If I use the Secured version IC - can I consider it as 100% drop-in-replacement for the non-secured version? I.e - same SW and same HW (of course, without using the secured features that exist only in S version). assuming of course, that I refer to same package (i.e LQFP100).&lt;/P&gt;&lt;P&gt;2. On top of the last question, can I also consider the&amp;nbsp;&lt;STRONG&gt;LPC55S69JBD100&lt;/STRONG&gt;&amp;nbsp;as a replacement for the&amp;nbsp;&lt;STRONG&gt;LPC55S28JBD100&lt;/STRONG&gt;&amp;nbsp;if I do not use the "extra features" that the S69 ofers (i.e - dual core dsp accelerator) ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. Can I say that those 3 components has actually same pin functionality assuming I use the basic (or common) funciality of the &lt;STRONG&gt;LPC5528JBD100&lt;/STRONG&gt;&amp;nbsp;? which is another way to say that the S28 and S69 are based on the 28 with additional features.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;LPC5528JBD100&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;LPC55S28JBD100&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;LPC55S69JBD100&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to understand if any pin definitions as GPIO/UART/SPI/etc will be different for each of the above.&lt;/P&gt;&lt;P&gt;4. For SW aspect - can I burn same code for S and non-S version if the security-features are not used? or it will require different compilation for each?&lt;/P&gt;&lt;P&gt;I'm referring to the the product family comparison where I see that the "security system" is considered as "optional", so I guess that the SW/HW can be developed with the secured version but is only optional to be actually used:&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc5500-arm-cortex-m33:LPC5500_SERIES" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc5500-arm-cortex-m33:LPC5500_SERIES&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Nov 2022 08:55:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC552x-S2x-S6x/m-p/1555668#M50742</guid>
      <dc:creator>Uzi</dc:creator>
      <dc:date>2022-11-17T08:55:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC552x/S2x/S6x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC552x-S2x-S6x/m-p/1557301#M50776</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203185"&gt;@Uzi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;I noticed that you have another similar case, so I will follow up on this last one that I mention.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Mon, 21 Nov 2022 17:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC552x-S2x-S6x/m-p/1557301#M50776</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-11-21T17:54:47Z</dc:date>
    </item>
  </channel>
</rss>