<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC845 DAC1 Configuration in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC1-Configuration/m-p/1546394#M50569</link>
    <description>&lt;P&gt;I am using the LPCXpresso845-MAX board and wish to use DAC1 which is connected to the speaker.&amp;nbsp; In the schematic for the board it shows that the speaker is connected to DAC1 via pin PIO0_29.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Referring to the LPC845 user manual UM11029 rev 1.7 of April 2021 I see that in the IOCON register for DAC0, PIO0_17, there is a DACMODE bit (number 16) that must be set to use DAC0, but in IOCON register for PIO0_29 there is no corresponding bit for DAC1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I set DACMODE for DAC1 in PIO0_29?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 31 Oct 2022 15:44:39 GMT</pubDate>
    <dc:creator>kk7xo</dc:creator>
    <dc:date>2022-10-31T15:44:39Z</dc:date>
    <item>
      <title>LPC845 DAC1 Configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC1-Configuration/m-p/1546394#M50569</link>
      <description>&lt;P&gt;I am using the LPCXpresso845-MAX board and wish to use DAC1 which is connected to the speaker.&amp;nbsp; In the schematic for the board it shows that the speaker is connected to DAC1 via pin PIO0_29.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Referring to the LPC845 user manual UM11029 rev 1.7 of April 2021 I see that in the IOCON register for DAC0, PIO0_17, there is a DACMODE bit (number 16) that must be set to use DAC0, but in IOCON register for PIO0_29 there is no corresponding bit for DAC1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I set DACMODE for DAC1 in PIO0_29?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 31 Oct 2022 15:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC1-Configuration/m-p/1546394#M50569</guid>
      <dc:creator>kk7xo</dc:creator>
      <dc:date>2022-10-31T15:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 DAC1 Configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC1-Configuration/m-p/1546701#M50586</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/172140"&gt;@kk7xo&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There isn't this bit, no need config&amp;nbsp;&lt;SPAN&gt;DACMODE bit.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Nov 2022 07:25:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC1-Configuration/m-p/1546701#M50586</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-11-01T07:25:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845 DAC1 Configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC1-Configuration/m-p/1549178#M50625</link>
      <description>Thank you!</description>
      <pubDate>Sat, 05 Nov 2022 16:33:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-DAC1-Configuration/m-p/1549178#M50625</guid>
      <dc:creator>kk7xo</dc:creator>
      <dc:date>2022-11-05T16:33:23Z</dc:date>
    </item>
  </channel>
</rss>