<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックWhat's the difference between the NHS3100 and LPC8N04</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-the-NHS3100-and-LPC8N04/m-p/1544671#M50517</link>
    <description>&lt;P&gt;I've compared these two offerings' datasheets, which look almost identical. Can someone point out what the difference is?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 27 Oct 2022 04:17:36 GMT</pubDate>
    <dc:creator>raven_coda</dc:creator>
    <dc:date>2022-10-27T04:17:36Z</dc:date>
    <item>
      <title>What's the difference between the NHS3100 and LPC8N04</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-the-NHS3100-and-LPC8N04/m-p/1544671#M50517</link>
      <description>&lt;P&gt;I've compared these two offerings' datasheets, which look almost identical. Can someone point out what the difference is?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 27 Oct 2022 04:17:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-the-NHS3100-and-LPC8N04/m-p/1544671#M50517</guid>
      <dc:creator>raven_coda</dc:creator>
      <dc:date>2022-10-27T04:17:36Z</dc:date>
    </item>
    <item>
      <title>Re: What's the difference between the NHS3100 and LPC8N04</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-the-NHS3100-and-LPC8N04/m-p/1544767#M50522</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I have to admit the two silicons are almost&amp;nbsp; the same from perspective of core, pin assignment, functions, features.&lt;/P&gt;
&lt;P&gt;But the MHS3100 has multiple packages, the LPC8N04 just has one package.&lt;/P&gt;
&lt;P&gt;Pls refer to section 7 Pinning.&lt;/P&gt;
&lt;P&gt;I attach the data sheet of both silicons.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Oct 2022 06:58:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-the-NHS3100-and-LPC8N04/m-p/1544767#M50522</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-10-27T06:58:32Z</dc:date>
    </item>
    <item>
      <title>Re: What's the difference between the NHS3100 and LPC8N04</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-the-NHS3100-and-LPC8N04/m-p/1545087#M50529</link>
      <description>&lt;P&gt;Thanks for the quick reply. I did notice the different footprint options for the NHS3100. If that's the only difference then I'll just assume the NHS3100 supersedes the LPC8N04.&lt;/P&gt;</description>
      <pubDate>Thu, 27 Oct 2022 14:09:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-the-NHS3100-and-LPC8N04/m-p/1545087#M50529</guid>
      <dc:creator>raven_coda</dc:creator>
      <dc:date>2022-10-27T14:09:38Z</dc:date>
    </item>
  </channel>
</rss>