<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Cannot flash LPC55S69J MCU in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-flash-LPC55S69J-MCU/m-p/1544550#M50516</link>
    <description>&lt;P&gt;We are having issues flashing the LPC55S69J MCU. Flashing is performed via SWD.&lt;/P&gt;&lt;P&gt;This is the error message the IDE shows: Wire ACK Fault in DAP access&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ay44_0-1666832523070.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/198278i3916AFE86CD3B3C3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ay44_0-1666832523070.png" alt="ay44_0-1666832523070.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;We've confirmed we have the right MCU orientation, correct voltages, etc. We are using the same setup that successfully flashes the&amp;nbsp;LPC55S69-EVK.&lt;/P&gt;&lt;P&gt;Is there a particular pin configuration needed for the LPC55S69 MCU to flash? Anything missing from the setup detailed?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;** Setup **&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Hardware platforms used:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;- Custom designed board&lt;BR /&gt;- Breakout board with LPC55S69J MCU soldered on (Digikey PN: PA0096-ND)&lt;BR /&gt;- MCU-LINK board&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Hardware notes:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;MCU: LPC55S69JBD64K&lt;/P&gt;&lt;P&gt;SWDIO: pulled up via 100k; connected to pin 5 of MCU&lt;/P&gt;&lt;P&gt;SWCLK: pulled down via 100k; connected to pin 6 of MCU&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;VBAT_PMU pulled high 3V3&lt;/P&gt;&lt;P&gt;Reset line observed high; pulls low from programmer&lt;/P&gt;&lt;P&gt;All VDD pins externally connected to 3V3&lt;/P&gt;&lt;P&gt;All VSS pins externally connected to ground&lt;/P&gt;&lt;P&gt;USB1 (high speed) used&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Setup information:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;NXP Eval kit used: LPC55S69-EVK&lt;/P&gt;&lt;P&gt;NXP Programmer: MCU-LINK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;PC/IDE info:&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;Product: MCUXpresso IDE&lt;/P&gt;&lt;P&gt;Version: MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13]&lt;/P&gt;&lt;P&gt;Operating system: Windows 10&lt;/P&gt;&lt;P&gt;VM: OpenJDK 64-Bit Server VM (64 bit)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NXP LPCXpresso55S69 Development Board: &lt;A href="https://www.nxp.com/design/development-boards/lpcxpresso-boards/lpcxpresso55s69-development-board:LPC55S69-EVK" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/development-boards/lpcxpresso-boards/lpcxpresso55s69-development-board:LPC55S69-EVK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NXP MCU-Link Debug Probe: &lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/mcu-link-debug-probe:MCU-LINK" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/microcontrollers-developer-resources/mcu-link-debug-probe:MCU-LINK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;Log information generated the IDE:&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.6 (Jul 12 2022 16:58:24 - crt_emu_cm_redlink build 4)&lt;/P&gt;&lt;P&gt;Found chip XML file in C:/ (&lt;EM&gt;&lt;STRONG&gt;removed&lt;/STRONG&gt;&lt;/EM&gt;)&lt;/P&gt;&lt;P&gt;(&amp;nbsp;&amp;nbsp;5) Remote configuration complete&lt;/P&gt;&lt;P&gt;Reconnected to existing LinkServer process.&lt;/P&gt;&lt;P&gt;Connecting to probe 1 core 0 (using server started externally) reports:&lt;/P&gt;&lt;P&gt;'Ee(42). Could not connect to core.'&lt;/P&gt;&lt;P&gt;Retrying...&lt;/P&gt;&lt;P&gt;Reconnected to existing LinkServer process.&lt;/P&gt;&lt;P&gt;Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.&lt;/P&gt;&lt;P&gt;Failed on connect: Ee(42). Could not connect to core.&lt;/P&gt;&lt;P&gt;No connection to chip's debug port&lt;/P&gt;</description>
    <pubDate>Thu, 27 Oct 2022 01:22:26 GMT</pubDate>
    <dc:creator>ay44</dc:creator>
    <dc:date>2022-10-27T01:22:26Z</dc:date>
    <item>
      <title>Cannot flash LPC55S69J MCU</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-flash-LPC55S69J-MCU/m-p/1544550#M50516</link>
      <description>&lt;P&gt;We are having issues flashing the LPC55S69J MCU. Flashing is performed via SWD.&lt;/P&gt;&lt;P&gt;This is the error message the IDE shows: Wire ACK Fault in DAP access&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ay44_0-1666832523070.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/198278i3916AFE86CD3B3C3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ay44_0-1666832523070.png" alt="ay44_0-1666832523070.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;We've confirmed we have the right MCU orientation, correct voltages, etc. We are using the same setup that successfully flashes the&amp;nbsp;LPC55S69-EVK.&lt;/P&gt;&lt;P&gt;Is there a particular pin configuration needed for the LPC55S69 MCU to flash? Anything missing from the setup detailed?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;** Setup **&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Hardware platforms used:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;- Custom designed board&lt;BR /&gt;- Breakout board with LPC55S69J MCU soldered on (Digikey PN: PA0096-ND)&lt;BR /&gt;- MCU-LINK board&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Hardware notes:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;MCU: LPC55S69JBD64K&lt;/P&gt;&lt;P&gt;SWDIO: pulled up via 100k; connected to pin 5 of MCU&lt;/P&gt;&lt;P&gt;SWCLK: pulled down via 100k; connected to pin 6 of MCU&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;VBAT_PMU pulled high 3V3&lt;/P&gt;&lt;P&gt;Reset line observed high; pulls low from programmer&lt;/P&gt;&lt;P&gt;All VDD pins externally connected to 3V3&lt;/P&gt;&lt;P&gt;All VSS pins externally connected to ground&lt;/P&gt;&lt;P&gt;USB1 (high speed) used&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Setup information:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;NXP Eval kit used: LPC55S69-EVK&lt;/P&gt;&lt;P&gt;NXP Programmer: MCU-LINK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;PC/IDE info:&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;Product: MCUXpresso IDE&lt;/P&gt;&lt;P&gt;Version: MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13]&lt;/P&gt;&lt;P&gt;Operating system: Windows 10&lt;/P&gt;&lt;P&gt;VM: OpenJDK 64-Bit Server VM (64 bit)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NXP LPCXpresso55S69 Development Board: &lt;A href="https://www.nxp.com/design/development-boards/lpcxpresso-boards/lpcxpresso55s69-development-board:LPC55S69-EVK" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/development-boards/lpcxpresso-boards/lpcxpresso55s69-development-board:LPC55S69-EVK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NXP MCU-Link Debug Probe: &lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/mcu-link-debug-probe:MCU-LINK" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/microcontrollers-developer-resources/mcu-link-debug-probe:MCU-LINK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;Log information generated the IDE:&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.6 (Jul 12 2022 16:58:24 - crt_emu_cm_redlink build 4)&lt;/P&gt;&lt;P&gt;Found chip XML file in C:/ (&lt;EM&gt;&lt;STRONG&gt;removed&lt;/STRONG&gt;&lt;/EM&gt;)&lt;/P&gt;&lt;P&gt;(&amp;nbsp;&amp;nbsp;5) Remote configuration complete&lt;/P&gt;&lt;P&gt;Reconnected to existing LinkServer process.&lt;/P&gt;&lt;P&gt;Connecting to probe 1 core 0 (using server started externally) reports:&lt;/P&gt;&lt;P&gt;'Ee(42). Could not connect to core.'&lt;/P&gt;&lt;P&gt;Retrying...&lt;/P&gt;&lt;P&gt;Reconnected to existing LinkServer process.&lt;/P&gt;&lt;P&gt;Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.&lt;/P&gt;&lt;P&gt;Failed on connect: Ee(42). Could not connect to core.&lt;/P&gt;&lt;P&gt;No connection to chip's debug port&lt;/P&gt;</description>
      <pubDate>Thu, 27 Oct 2022 01:22:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-flash-LPC55S69J-MCU/m-p/1544550#M50516</guid>
      <dc:creator>ay44</dc:creator>
      <dc:date>2022-10-27T01:22:26Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot flash LPC55S69J MCU</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-flash-LPC55S69J-MCU/m-p/1544792#M50523</link>
      <description>&lt;P&gt;Hi&amp;nbsp;ay44&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12325.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12325.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;to design LPC55S69 DCDC&lt;/P&gt;
&lt;P&gt;This post includes DCDC circuit detection.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC55xx-Power-Supply-Circuit-Design-and-Detection-Method/ta-p/1429011" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC55xx-Power-Supply-Circuit-Design-and-Detection-Method/ta-p/1429011&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;For SWD interface design, please refer&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Oct 2022 07:16:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-flash-LPC55S69J-MCU/m-p/1544792#M50523</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-10-27T07:16:40Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot flash LPC55S69J MCU</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-flash-LPC55S69J-MCU/m-p/1564782#M50942</link>
      <description>&lt;P&gt;Hi Jun Zhang,&lt;/P&gt;&lt;P&gt;Thank you for the reply. I was able to get the MCU to flash. We provided VDD_PMU with 1.1V and flashing worked after this.&lt;/P&gt;&lt;P&gt;Our application does not use the internal DCDC converter. Could you confirm if the LCP55S69 MCU will function correctly if we do not use the built in DCDC converter and just supply VDD_PMU pin with 1.1V?&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 00:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-flash-LPC55S69J-MCU/m-p/1564782#M50942</guid>
      <dc:creator>ay44</dc:creator>
      <dc:date>2022-12-06T00:59:35Z</dc:date>
    </item>
  </channel>
</rss>