<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Unused USB pins</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unused-USB-pins/m-p/1541587#M50463</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Please use the DS recommended design for unused USB pins. This is related with on chip HW design.&lt;/P&gt;&lt;P&gt;y&lt;SPAN&gt;ou should consider USB low power mode or disable USB domain to lower the power consumption.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 21 Oct 2022 03:47:22 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2022-10-21T03:47:22Z</dc:date>
    <item>
      <title>Unused USB pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unused-USB-pins/m-p/1537120#M50397</link>
      <description>&lt;P&gt;Regarding the USBn_3V3 pins, the datasheet says "Tie to VBAT_DCDC or connect to ground . If not using USB and using 1.8 V supply, USBn_3V3 can be connected to 1.8 V." This is confusing. If you are not using USBn, and it says it can be connected to ground, then why not connect it to ground (to minimize supply current)?&lt;/P&gt;</description>
      <pubDate>Thu, 13 Oct 2022 12:46:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unused-USB-pins/m-p/1537120#M50397</guid>
      <dc:creator>jpowning</dc:creator>
      <dc:date>2022-10-13T12:46:09Z</dc:date>
    </item>
    <item>
      <title>Re: Unused USB pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unused-USB-pins/m-p/1540082#M50449</link>
      <description>&lt;P&gt;Hi&amp;nbsp;jpowning&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What's the part number?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 11:51:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unused-USB-pins/m-p/1540082#M50449</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-10-19T11:51:55Z</dc:date>
    </item>
    <item>
      <title>Re: Unused USB pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unused-USB-pins/m-p/1541269#M50459</link>
      <description>&lt;P&gt;Hi - the part I am using is LPC55S16JBD100. Thanks for your interest.&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 15:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unused-USB-pins/m-p/1541269#M50459</guid>
      <dc:creator>jpowning</dc:creator>
      <dc:date>2022-10-20T15:32:02Z</dc:date>
    </item>
    <item>
      <title>Re: Unused USB pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unused-USB-pins/m-p/1541587#M50463</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Please use the DS recommended design for unused USB pins. This is related with on chip HW design.&lt;/P&gt;&lt;P&gt;y&lt;SPAN&gt;ou should consider USB low power mode or disable USB domain to lower the power consumption.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Oct 2022 03:47:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unused-USB-pins/m-p/1541587#M50463</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-10-21T03:47:22Z</dc:date>
    </item>
  </channel>
</rss>